Part Number: TMS320C5505 Hi Team,
We are using TMS320C5505AZCH15 in our project . Since the operating temperature is only upto 70°C ,we want to know the options to read the die temperature from the DSP.
Our PCB is getting too hot because of other…
Part Number: TMS320C5505 I have a problem to multiply the variables x and y and save the result to z. I tried to use the MPY directive. I am using a TMS320C550 processor and I have to write it in assembly
.data x
.word 0x1000
y .word 0x2000
z .word …
Part Number: TMS320C5505 Customer wants to use byte-mode to save memory, but I see in compiler readme only C55+ core support byte-mode, but did not say which device is C55+ core
In C5505 datasheet, the CPU is V3.3, not mention plus, which device used…
Part Number: TMS320C5505
Hello Guys,
Good day.
Our customer needs the documents for C5500 Code Generation Tools v4.4.2 (Defect History, Linker Notes, Release Notes and C55x+ Notes). They need this documents to update some documentations for the tools they…
Part Number: TMS320C5505 Tool/software: Code Composer Studio I'm a CSULB Electrical Engineering student taking a course in DSP Design ( EE489: Digital Signal Processing Design ), and a problem I'm encountering with my TMS320C5505 and Code Composer Studio…
Part Number: TMS320C5505 Tool/software: Code Composer Studio I'm following a tutorial from a book which uses an older version of CCS which has the "Texas Instrument XDS100v2 USB Emulator". The TMDX5505EZDSP support page says the board has…
Part Number: TMS320C5505 Tool/software: Code Composer Studio Hi,
The TMS320C5505 data sheet shows that the maximum operating frequency of EM_SDCLK is 50 MHz when DVDDEMIF = 1.8 V, as shown in the figure below. Does this mean that the operating frequency…
Part Number: TMS320C5505
Tool/software: TI C/C++ Compiler
I had converted a .pcm file to a .wav file and knows how it sounds. After I converted the .pcm file to a .csv file and read the .csv file's graph as a representation of the sound file's sound…
Part Number: TMS320C5505 Hi TI Experts,
Customer board using C5505 suffers from garbling UART. (It's based on USBSTK5505) It occurs in 2 out of 10 units.
Environment ・ UART Baudrate 115200 ・ CLKIN 18.432MHz ・ PLL 18.432 / 384 * 2500 = 120MHz
When checking…
Part Number: TMS320C5505 Tool/software: Code Composer Studio Hello i'm working on building a low power Digital hearing aid like the one in Application Report SPRA657 April 2000,
All the parts seem to obsolete TMS320C5000
I'm wonder if i can receive…