Part Number: TMS320C5517
Tool/software:
Hi Expert,
My customer wants to know ROM at TMS320C5517 can storage data more than 10 years or not. Do you have some document which guarantee it? This is because EE at customer needs to standard or not on…
Part Number: TMS320C5517 Tool/software: Dear TI Support Team,
I am using the following setup to read microphone data:
Processor Board : TMS320C5517 EVM
Audio Front-End : PCM1864CMBEVM (TIDA-01454B)
Demo Used : BF_rt_bios from C:\ti…
Part Number: TMS320C5517 Other Parts Discussed in Thread: TIDA-01454 , , PCM1864 Tool/software: Dear TI Support Team,
I am currently working with the following setup:
Audio Input Board : PCM1864CMBEVM with TIDA-01454 Rev B
DSP Platform …
Part Number: TMS320C5517 Tool/software: Dear TI Support Team,
I am currently working with the TMS320C5517 EVM and evaluating the USB functionality using the example projects provided in the C5517 USB software package (e.g., WINUSB, HID, MSC examples…
Part Number: TIDA-01589 Other Parts Discussed in Thread: TMS320C5517 , Dear TI Support Team,
We are currently using TMS320C5517 in our design (reference: TIDA-01589) and require Ethernet connectivity for streaming processed data.
We would like your…
Part Number: TMS320C5517 Tool/software: Hi, I'm trying to display text messages on the console window using printf(); under running by "Select program to load",but not work like as under Debug mode.Is any operation needed to printf() be availableon the…
Part Number: TMS320C5517 Other Parts Discussed in Thread: TIDA-01589 ,
Hi,
We are looking into developing a Hands-free Intercom by utilizing a design similar to TIDA-01589.
The specification for the hands-free Intercom are as follows:
Interfaces…
Part Number: TMS320C5517 Hi everyone.
In my application we intend to use a 16-bit NOR Flash, to boot and then make it usable for the program DSP, via EMIF. As regards the connection of addresses, the "spruh16b" datasheet on page 221 recommends the connection…
Part Number: TMS320C5517 Tool/software: Hi,
Could you let me know the reason why SW reset, asm(“RESET”) does not work in my code placed on flash? The code can work well in debug mode.
I expect that you have already had the experience to see this phenomenon…
Part Number: TMS320C5517 Tool/software: Hi,
I am planning to use TMS320C5517 but it is not clear if internal ROM can be used for the booting directly without any external peripherals.
Request you to clarify.
Regards,
Anurag