Part Number: TMS320C5517 Tool/software: Hi,
I am planning to use TMS320C5517 but it is not clear if internal ROM can be used for the booting directly without any external peripherals.
Request you to clarify.
Regards,
Anurag
Part Number: TMS320C5517 Other Parts Discussed in Thread: ADS1299 Tool/software: Hi Everyone,
I have a problem reading data from a slave device (ADS1299 converter) on the SPI RXx register using the fifo buffer in reception only. Basically I am receiving…
Part Number: TMS320C5517 Tool/software: I'm interested in using this chip on a new design. The eval boards are obsolete and no longer manufactured.
I'm hoping someone has an old one lying around collecting dust.
Thanks.
Part Number: TMS320C5517 Tool/software: Hello,
I am reading TMS320C5517 data sheet, SPRS727C –AUGUST 2012–REVISED APRIL 2014.
I am searching VIH and VIL of I2C pins.
I found VOH and VOL in page 59, but I can not find VIH and VIL.
Could you…
Part Number: TMS320C5517 Other Parts Discussed in Thread: TIDA-01589 ,
Hi,
We are looking into developing a Hands-free Intercom by utilizing a design similar to TIDA-01589.
The specification for the hands-free Intercom are as follows:
Interfaces with…
Part Number: TMS320C5517 Other Parts Discussed in Thread: DAC80501 Tool/software: Hi everyone, I would like to perform I2c writes using the DMA from my TMS320C55517 DSP (master) to the DAC80501M peripheral (slave). I want to use DMA on the I2c bus because…
Part Number: TMS320C5517 "Supply voltage, Digital Core Slew rate < 200us for full swing"is written in the TMS320C5517 datasheet page58. Does this mean that CVDD should start up from 0V to 1.4V (1.3V, 1.05V) within 200us?
Best regards.
Part Number: TMS320C5517 Tool/software: Hi,
I would like to know of possible causes for the transmitter holding register empty interrupts no longer being received after a certain time from starting the app ?!
Essentially, I have configured the UART on…
Part Number: TMS320C5517 Hi everyone.
In my application we intend to use a 16-bit NOR Flash, to boot and then make it usable for the program DSP, via EMIF. As regards the connection of addresses, the "spruh16b" datasheet on page 221 recommends the connection…