Part Number: TMS320C5517 Hi, My customer reported an issue related I2S receive. I2S is connected with FPGA. DSP and I2S configurations are below: DSP clock = 172.8MHz (w/ 19.2MHz source) I2S0 is used. I2S configuration: MONO = 0 (Stereo) LOOPBACK = 0 (disabled…
Part Number: TMS320C5517 I want to integrate an eMMC in a project to save monitoring data. The TMS320C5517 work on 4.3 eMMC compliance, so it should work with eMMC 5.1
can it work at high speed SDR or just legacy mmc ? What is the maximum supported memory…
Part Number: TMS320C5517 Other Parts Discussed in Thread: TIDA-01589 , TIDEP-0077 Hi Team,
My customer used TMS320C5517 on audio conference system application, and would like to request the example code on the AEC algorithm.
The algorithms used are based…
Part Number: TMS320C5517
Hi Team,
Is the TMS320C5517AZCH20 SMD type or NSMD type?
Also, Could you tell me the dimension information of (A) to (C)?
Your prompt support would be highly appreciated, thank you!
Part Number: TMS320C5517
I am doing doing updates to a project that uses the TMS320C5517. Previously I was using CCS5.5 with DSP/BIOS.
I saw that it is recommended to move from DSP/BIOS to SYS/BIOS.
1. What version of SYS/BIOS is recommended for this…
Part Number: TMS320C5517
Hello team,
Let me ask a couple of questions regarding thermal design guideline.
1) Is there a recommended Tj(max) range for this device? (We can find 150C max as Tstg but not for operation ratings description on the datasheet…
Part Number: TMS320C5517 The serial NOR flash memory MT25QL256ABA8E12 is compatible with DPS MT25QL256ABA8E12 in McSPI boot Mode?
if no, is there other Serial NOR flash for recommend?
Hi Frank ,
Thank you for your help!
"capturing the ALC output can show whether ALC is doning the work or not ",I 'll check it later.
Best Regard!
Dudechao