Part Number: TMS320C5517 Hello Champs, HW: Customer own C5517 board SW:C:\ti\c55_lp\c55_csl_3.08\ccs_v6.x_examples\programmer Customer could burn <64K bin file to NAND flash, but failed to burn >64K size. He tracked the code in nand_flash.c, the fread…
Part Number: TMS320C5517 Hi,
I have a question about C5517 EM_WAIT pins.
The question is about the description of CS2_WAIT - CS5_WAIT which are written in C5517 Technical Reference Manual (SPRUH16B) page.253 "4.4.4 AWCCR2 Register (offset = 1005h) [reset…
Part Number: TMS320C5517 Hello,
According toTMS320C5517 technical reference manual (SPRUH16B) "Table 1-59. LDO Controls Matrix" page 125:
Setting BG_PD bit or LDO_PB bit in RTCPMGT register (1930h) should enable to shut down on_chip LDO. (in my…
Part Number: TMS320C5517 Hello!
I would like to connect the McBSP of the TMS320C5517 on the Evalboard to an external PCM32 port with it's external Clocks.
The FSX/FSR is an symmetric Clock of 8kHz an the Bitclock CLKR is 4096kHz Doubleclock. There…
Hi Frank!
Frank Livingston said: Did you get the 2x EP1 interrupts every 1 msec without IAD?
Yes, I checked it. I checked PERI_TXCSR register: ISO mode == 0. Why? I set it via USB_configEndpt().
Checked UNDERRUN bit, everything is fine in any situation…
Part Number: TMS320C5517 Hi team,
My customer have the question about C5517, can you please help me with it?
I found this thread https://e2e.ti.com/support/processors/f/791/t/602119
We use TMS320C5517 DSP and c55_csl_3.08.01 / DSPBIOS bios_5_42_02_10 in…
Part Number: TMS320C5517 Hi Experts,
Our customer was developing their system with TMS320C5517. For their system, they are using External clock input dn the desired SYSCLOCK is generated by PLL/CLOCK Generator. If there are some omission/toothless clock…
Part Number: TMS320C5517
Hello,
In the TMS320C5517 Fixed-Point Digital Signal Processor datasheet ( https: //www.ti.com/lit/ds/symlink/tms320c5517.pdf )
p20/193, we can read for EM_WAIT2 pin that The IPD resistor on this pin can be enabled or disabled…
Hello, Mr. Ming.
This is Nakahara, who was posted on the forum by Mr. Miyazaki.
Sorry for the late reply.
Thank you for your comments.
1. I checked the map file, but SARAM31 (byte address 0x4E000 – 0x4FFFF) looks unused.
2. I tried adding the…