Part Number: TMS320C5517 Hi team,
My customer have the question about C5517, can you please help me with it?
I found this thread https://e2e.ti.com/support/processors/f/791/t/602119
We use TMS320C5517 DSP and c55_csl_3.08.01 / DSPBIOS bios_5_42_02_10 in…
Part Number: TMS320C5517 Hello!
I would like to connect the McBSP of the TMS320C5517 on the Evalboard to an external PCM32 port with it's external Clocks.
The FSX/FSR is an symmetric Clock of 8kHz an the Bitclock CLKR is 4096kHz Doubleclock. There…
Hi Frank!
Frank Livingston said: Did you get the 2x EP1 interrupts every 1 msec without IAD?
Yes, I checked it. I checked PERI_TXCSR register: ISO mode == 0. Why? I set it via USB_configEndpt().
Checked UNDERRUN bit, everything is fine in any situation…
Part Number: TMS320C5517
Hello,
In the TMS320C5517 Fixed-Point Digital Signal Processor datasheet ( https: //www.ti.com/lit/ds/symlink/tms320c5517.pdf )
p20/193, we can read for EM_WAIT2 pin that The IPD resistor on this pin can be enabled or disabled…
Part Number: TMS320C5517 Hi Experts,
Our customer was developing their system with TMS320C5517. For their system, they are using External clock input dn the desired SYSCLOCK is generated by PLL/CLOCK Generator. If there are some omission/toothless clock…
Hello, Mr. Ming.
This is Nakahara, who was posted on the forum by Mr. Miyazaki.
Sorry for the late reply.
Thank you for your comments.
1. I checked the map file, but SARAM31 (byte address 0x4E000 – 0x4FFFF) looks unused.
2. I tried adding the…
Part Number: TMS320C5517 Other Parts Discussed in Thread: TXB0104 , Dear Sir:
Please help check what the drive current of tms320c5517 is? Is it above +/- 2mA? we plan adding TXB0104 as the level shifter of I2S, thanks
Part Number: TMS320C5517 Other Parts Discussed in Thread: SPRC133 Hi All:
I inherited a C5517 EVM board. I'd like to play with some of it's functionality in CCS10.
Where can I find the test/demo software that (was possibly) part of this board? …
In the description of the CSL library for audio DSP ( https://www.ti.com/tool/SPRC133 ), support for the USB Audio Class Driver is declared, this information does not correspond to reality, since the number of errors found suggests that this often of your…
Part Number: TMS320C5517 Dear Sir:
the structure of out circuit as below, we need connect tms320c5517(1.8V) to other IC(3.3V), so we need adding levle shifter for I2S and UART, do you has suggestiong for these two kinds level shifters?
Thanks.... …