Other Parts Discussed in Thread: TMS320C5533 I would like to update a design that uses the TAS102B, but I am unable to find the TAS1020FDK. Is it still available?
Other Parts Discussed in Thread: PCM5242 , DIR9001 , PCM2706C , TMS320C5533 , PCM5122 , PCM5102 Hello,
are there linux drivers available for the PCM5242?
can we see the gerber file for it?
thank you
Michael Carrier said: We are using CCS 5.4. So the device ID that CCS is expecting is something like TMS320C5533?
Well it is looking for some value but it won't be obvious like TMS320C5533. It'll be like 0x4C or something like that.
I wondering…
Hi Arjun,
As you mention, the TAS1020B is Not Recommended for New Designs. The replacement for this device is the TMS320C5533, you may take a look at this wiki that explains the differences between these devices:
http://processors.wiki.ti.com/index.php…
Hi Charlie,
An I2S to USB interface can be a combination of USB codec like PCM2902C with S/PDIF input and DIT4096 which converts I2S to the S/PDIF.
Another option is to use TMS320C5533 which is the replacement part for TAS1020B.
Best regards,
Ivan…
Other Parts Discussed in Thread: TMS320C5533 Hi,
Any tip for a multichannel usb to i2s ic?
i've looked at http://www.ti.com/product/tms320c5533/description but it has only 4 I2S channels and i need at least 8.
Thank you in advance
Hello Matsumoto-san
Please notice that the TUSB3200 is Not Recommended for New Designs (NRND), the replacement part is the TMS320C5533.
Best regards,
Diego.
Other Parts Discussed in Thread: TMS320C5533 I'm making a DAW to be connected to a USB device. The analog source and destination are 1/4 inch analog jacks. I would like the device to be full-duplex, USB compatible with windows, and 24 bit audio, at least…
Hi, Jerry,
Yes, you need some sort of chip to do this. For example, we recommend customers to use something like this: http://www.ti.com/product/tms320c5533/description
-d2