Hi Kaka-San,
These devices are very similar with minor differences as memory size or DMA channels. I must point out that these devices are quite old and we are not longer recommending them for new designs, so the support will be limited. The suggested…
Hello, Mahesh,
There's no problem to play a file with a higher sample frequency. I mean, if the audio file was sampled at 8kHz, there's no problem to use a higher sample frequency such 48kHz. It must not be lower than 8KHz.
The .wav or .mp3…
Hi d2
I also started with the Evaluation Stick with the TLV320AIC3254 and the TAS1020B Streaming Controller. Now I am looking for an other Streaming Controller, because the TAS1020B is NRND. Is there a possibility to convert the Firmware from TAS1020B …
Hi,
The TMS320C5532, TMS320C5533, TMS320C5534 and TMS320C5535 are the industry’s lowest cost and lowest power 16-bit processors helping conserve energy at exceptional levels and enabling longer battery life.
Whereas, The TMDX5535eZdsp is a small…
Other Parts Discussed in Thread: TMS320C5533 Hi,
How can one predict how much RAM a particular embedded system needs? I am using the TMS320C5533 processor with 128KB RAM. However, I need to implement peripherals such as SD/MMC + FAT fs, HS USB, as well…
Other Parts Discussed in Thread: PCM2902C , TMS320C5533 , DIT4096 Are there any products that will allow me to send 24 bit/48 kHz stereo I2S data over usb? I am trying to record audio data on a PC so it will only need to be I2S to USB, not USB to I2S.
…
Hi Martin,
I have only experience with onboard S/PDIF output which can send DTS. Any simple USB codecs probably doesn't have this possibility. First try to read USB audio class 2.0, because it is possible that you can't do it with standard USB audio drivers…
Other Parts Discussed in Thread: PCM5242 , PCM1794A , TPA6120A2 , OPA2134 , TL072 , OPA4134 , PCM1792A , PCM2706C , TMS320C5533 Hi,
I am planning to design a portable USB-DAC, I can't decide which dac chip to use.
ti pcm5242, ti pcm1794a , wolfson wm8741 …
Other Parts Discussed in Thread: TMS320C5533 Hi!
I have USB Audio sound card based on TUSB3200C.
I want to redesign it and use new chip, because TUSB3200 is NRND now. Product page http://www.ti.com/product/tusb3200 recommends to use TMS320C5533.
Can this…