Part Number: TMS320C5535 We have designed a device that contains two C5535s running at 100MHz and use the USB i/f of each processor.
We use the USB boot mode to load our firmware
We have seen issues with the USB port not being recognized by the host. …
Part Number: TMS320C5535 OS: Windows 11 Pro
CCS Compiler version: CCS Version 12.1 (Latest)
We are using TMS320C5535 eZdsp Kit for demonstration of audio example in windows 11. But the USB port is not detectable by the system, also find the same error…
Part Number: TMS320C5535 We're running Code Composer Studio version 6.2 on Windows 11. We selected this version for its support of both the C55xx family of DSPs and the XDS100v2 JTAG probe.
Currently, we are unable to load .out files via JTAG to…
Part Number: TMS320C5535 Other Parts Discussed in Thread: SPRC133 , SYSCONFIG I have a similar issue to the previous thread.
I am using CCS v10.1.1, compiler V4.4.1 and Bios v5.42.1.09. I am building a project that I inherited form another developer that…
Part Number: TMS320C5535 Hi,
I remember the IDE on the CCS3.3 allowed the setting (toggle ON/OFF) of Line Markers , which one could scatter about on a page of code, and jump/cycle from one marker to another with the simnple press of a key short-cut. This…
Hi Wei,
Yuankai Zhang said: 3 twiddles, 1024 -pt ,2048 -pt ,4096 -pt , to save resources
The twiddles are e^(-j*2*pi/N). For an N-point FFT, a single size N/2 twiddle table is required. The twiddles for smaller size FFTs are contained in this twiddle table.…
Part Number: TMS320C5535 hi, While bring up C5535 USB audio streaming demo, in the Windows 10, the USB device is not initialized. Our audio demo documentation mentions that it was tested on Windows 7. Do we need any additional steps to get this working…
Part Number: TMS320C5535 Other Parts Discussed in Thread: TMDX5535EZDSP I'm designing a product based on the C5535.
The datasheet notes the required sequencing of the USB supplies:
1. USB_VDDA1P3 and USB_VDD1P3 2. USB_VDDA3P3 3. USB_VBUS
The TMDX5535EZDSP…
Part Number: TMS320C5535 2768.error.docx
We are using TMS320C5535 eZdsp Kit, for testing audio example, this is the error its showing (error is in the attachment).
Part Number: TMS320C5535 In the C5535 datasheet it says
:For detailed information on eMMC boot partition, eMMC, SD, or SDHC and UART or USB boot modes, contact your local sales representative.
Can we obtain this information?.
thanks