Part Number: TMS320C6454 Good day,
I would like to find out what would make the top late to dislodge in the device and the marking to be removed all together.
TMS320C6454BGTZA
Part Number: TMS320C6454 Hi,
We are using TMS320C6454BCTZA in our new design, can you please support us by providing the evaluation board schematic for our reference.
Request you to help us out with design details for TMDSDSK6455 EVM board.
…
Part Number: TMS320C6454 The C6454 comes in three speed grades (720MHz, 850MHz, and 1GHz). The datasheet lists the nominal core voltage as 1.20V for the 720MHz and 850MHz speed grades and 1.25V for the 1GHz speed grade. Is it okay to run the 1GHz speed…
Part Number: TMS320C6454 Hi Experts, There is no CTZ drawing in https://www.ti.com/packaging/docs/searchtipackages.tsp?packageName=BGA .
I would like to check the differences between TMS320C6454BCTZA and TMS320C6454BZTZ. TMS320C6454BCTZA Package CTZ…
Part Number: TMS320C6454 For more then 15 years we use same design same code
We are using tms320c6454 dsp in McBSP
We use Dx0 as data output
Clk0 as sync clock output
Clkr0 as output gpio
Fsro as input gpio
Dr0 as output gpio
While…
Other Parts Discussed in Thread: TMS320C6454 Hi,
I want to confirm the CVDD Condition for TMS320C6454.
SPRS311I (6.2 Recommended Operating Conditions) Mentioned CVDD as
Following.
1000 MHz → 1.25V
850 MHz → 1.20V
720 MHz → 1.20V…
Other Parts Discussed in Thread: TMS320C6454 I'm using TMS320C6454 processor. When I build a project, I get an error like this:
fatal error: #error NO CHIP DEFINED (use -dCHIP_XXXX where XXXX is chip number, i.e. 6201)
Settings in Build Options is…
Other Parts Discussed in Thread: TMS320C6454 Hello,
As a cost reduction I am to find a drop in replacement part for TMS320C6454, is there one I can use that is fully compatible with TMS320C6454. This part has been on the design for a long time and the…