Part Number: TMS320C6457 Hello ,
During a DPA of TMS320C6457CGMHA, LDC 1040 the following issues were found. Please provide feedback.
Voids were found in the heat spreader attach, diebumps, and board vias.
Thanks
…
Part Number: TMS320C6457 Hi,
In the development project, rapidio is required to implement 5Gbps link transmission in X1mode. Currently, the parallel image data input to DSP is 8bit@100MHZ, so a DSP with low power consumption needs to be selected, please…
Part Number: TMS320C6457
Hi Team, seeking for some support.
During power application to the DSP TMS320C6457 the POR and the Reset pins are asserted Low. After stable power is applied, should the POR pin and the RESET pin be deasserted at the same…
Part Number: TMS320C6457 I'm searching if any SYS/BIOS or TI-RTOS supports the TMS320C6457 in the Code Composer Version 9.3. When I go in the C6457 related page under development kit I end up on a download page where I can't see
any available link.…
Part Number: TMS320C6457 Hello,
I have a new project to develop which is based on an old DSP: the tms320c6457.
In the past I had projects based on CCS 3.3 environment and DSP BIOS 5.33.06 for the same DSP. But now I would like to upgrade to a more…
Part Number: TMS320C6457 Hello, My customer would like to know the Internal Pull-Up and Pull-Down resistor value as follows. Q1: How much ohms is the internal Pull-Down resistor at TRST pin? Q2: How much ohms is the internal Pull-Pu resistor at TDI, TMS…
Part Number: TMS320C6457 Tool/software: Code Composer Studio I have a program that doesn't work with dhcp.
"Running" doesn't go any further.
The request does not come to the host machine where the DHCP server is installed.
2020.09.14 17:51:02…
Part Number: TMS320C6457 Other Parts Discussed in Thread: SYSBIOS Hi,
If the Ethernet MAC of TMS320C6457 is driven by system/bios, and which is embedded in TI DSP?
Thanks.
Derek
Part Number: TMS320C6457 Hi Team,
Could you tell me the maximum power consumption of the resistors connected to the PTV18 pin?
Also, what is the recommended power rating of the resistor?
Best regards, yoshi.
Part Number: TMS320C6457 Good mornig,
i've a problem with CCS 8.3.1 during Platform addition.
In particoular, i've define a pltafor in a specific folder of my project and it is not listed il a drop down list of platform in build settings General Platform…