Other Parts Discussed in Thread: TMS320C6474 , TMS320C6678 Hi,
We are currently working with board level Power integrity analysis for the Cvdd rail (.9Volt). Based on the guidelines we have selected the Decoupling capacitors with Low ESR and low ESL valued…
Hi, guys! I'm trying to build a connection between PC and C6474 EVM with cable, so I download NDK2.0.0 and I am puzzled with the client example because it seems that it wants to fulfill a lot of thing, which makes the code hard to understand in return…
We are working on the implementation of TCP2 based decoder on the 6474 processor according to the LTE protocal. we want to decode the data after de-ratematching on the PUSCH and the transport block size is given by table 7.1.7.2.1-1 (3GPP TS 36.213…
Other Parts Discussed in Thread: TMS320C6474
Hi,
I use a EVM TMS320C6474,
my CCS version is: 5.0.3
I setup an new target configuration and launch, when I connect target, there is a error:
IcePick_C_0: Error connecting to the target: (Error -151)…
Other Parts Discussed in Thread: CCSTUDIO , OMAP-L137 hello,
I am using the board for the first time. i FOLLOWED SOME BOOKS ABOUT C6XXX PROCESSORS and everytime i get errors about the memory . can somebody please tell me how to write the command file to…
Hello,
I'm presently working on the same Evaluation module, i was wondering if you could help me with it. I'm actually implementing a waveform on the module and i need to know how the aif module works with edma and interrupt module. I tried to search…
Other Parts Discussed in Thread: TMS320C6474 Hi All, we are developing custom board using TMS320C6474 DSP,SRIO implementation with IDT TSI578 SRIO Switch. We have used 6 TMS320C6474 dsp's on board and they are connected to one SRIO switch. Assuming Dev…
Other Parts Discussed in Thread: TMS320C6474 hi
i am having some problems in some of the TMS320C6474 which i work on and i think the source for this problems is the ddr memory ,the reason for that because i ran the code for testing the ddr which came…
Other Parts Discussed in Thread: TMS320C6474 I am a new DSP user, i need to UART communication TMS320C6474 EVM with computer over USB, but i couldnt find any UART source code for 6474, and i looked for UART module in 6474 datasheet, i couldnt see any uart…