Part Number: TMS320C6652 Hi,
I have a question about SPI Boot of C665x. The setting of the BOOTMODE pin can change the parameter table index, does this mean that the user can have multiple application images to launch with this pin setting?
Best Regards…
Part Number: TMS320C6652 Hi,
We are using TMS320C6652.
Need to know if we can leave these signals unconnected or should we consider this signals during Boot mode.
PCIESSMODE[1:0]/GPIO[15:14], and PCIESSEN/TIMI0)
These signals are mentioned as reserved…
Part Number: TMS320C6652 Hi,
Can we configure the GPIO1:13 pins as GPIOs after the BOOT up.
Does the primary functions of these pins are BOOT config pins ?
Regards,
Divy
Part Number: TMS320C6652 Hi,
From the keystone Hardware guide, it is mentioned that unused LVDS clock can be terminated.
So is that the same case with DDRCLK ? I am not using DDR for processor .
Datasheet Pg 73 Power sequencing shows the DDRCLK . Does…
Part Number: TMS320C6652 Other Parts Discussed in Thread: LM10011 , TPS544C25 , Hi ,
I am planning to use TPS544C25 and LM10011 to power up TMS320C6652.
I understand from Datasheet the CVDD nominal voltage at start up is 1.1V. Please clarify the followi…
Part Number: TMS320C6652 Tool/software: TI C/C++ Compiler The C6652 DSP has no Ethernet port, can it be programmed only through the Jtag port? Is there any other way available?
Part Number: TMS320C6652 Leakage voltage appears at DVDD15 , it may come from CVDD1 via TMS320C6652. If this leakage needs to resolve, could you give me some advice?
TMS320C6652 power up sequence.pptx
Part Number: TMS320C6652 Other Parts Discussed in Thread: LM10011 TMS320C6652 requires 1.1V as the initial CVDD voltage at power on. I want to know the spec. I think that it will be 0.85V ~ 1,1V or 1,1×0.95V ~ 1.1V×1.05V.