Part Number: TMS320C6701 Tool/software: Code Composer Studio
Hi Expert,
I used CCS tool for TMS320C6701, but met below issue.
Where do I download DSP/BIOS tool?
CCS Version : 8.2
Compiler Version : 7.4
Part Number: ADS1282 Tool/software: Code Composer Studio Dear Chris, A few more questions on ADS1282. 1. What is the maximum value of series resistor that can be put in series with Ch1 and Ch2 positive inputs (AINP1 and AINP2) with their -ve inputs (AINN1…
Part Number: TMS320C6701 Dear All,
For X-ray medical equipments I'm re-enginering the electronic boards of a product designed almost 20-years ago. One of these boards has on it a floating-point DSP TMS320C31. This component is obsolete by long time…
Hi Pradeep,
Not a problem!
I would recommend tying the SYNC pin high to ensure that the the ADC is converting and that you can issue the "SYNC" SPI command and calibration commands (which require the SYNC pin to be high). If SYNC is left floating it…
Part Number: TMS320C6701 Hi,
Is there someone on this forum that would be able to answer the TMS320C6701 question asked on the following E2E thread?
Thanks, Chris
Part Number: TMS320C6701 Other Parts Discussed in Thread: SPRC090 , Hello,
The DSP/BIOS Driver Development Kit product bulletin (sprt261.pdf) says that the Driver Development Kit can be downloaded from this old non-functional link: www.ti.com/driverdevkit…
Part Number: TMS320C6701 This is an existing design so design changes are not doable.
Using the CCS emulator, I can write individual bytes in the SRAM.
But when I step thru the secondary bootloader's copy table code, it writes the same byte to all 4 bytes…
Part Number: TMS320C6701 Hi Team,
my customer is looking for an Asynchronous Memory Cycle Timing Diagramm for DMA (Burst) reads or writes from an Dual Port Memory with ARDY Output. They use an asynchronous SRAM Interface with ARDY Input to C6701 and burst…
Part Number: TMS320C6701
Tool/software: TI C/C++ Compiler
Team,
The CGTools 4.x for C6701 were provided as part of CCS 2.20.
Is there a way to use this compiler version on a newer CCS version like CCS 3.30 or CCSv4? How? I know that C6701 is not supported…