Part Number: TMS320C6713B Code composer version 12.7 I an trying to load an earlier compiler (which I have previously completed. I repeatedly get the followingt error.
I am using Help->Install code generation..
Unable to read repository at http:/…
Part Number: TMS320C6713B Trying to import a code composer 5.2 projects into 12.7... I already set the correct compiler (thanks for that in my last request), When I go to import the projects only one of them imports. The first time it happened I deleted…
Part Number: TMS320C6713B Tool/software:
On code composer 6, I accidentally selected the don't ask which project to load. Can someone point me to the location where I can clear this?
Thanks in advance.
Part Number: TMS320C6713B Plexus purchased these parts from Ti directly under PO: 12051325. The raw part's internal structure shows crack-like symptom. Are these actual cracks or delamination?
Ti lot#: 5483625WCW
DC: 2538
Part Number: TMS320C6713B Other Parts Discussed in Thread: TPS54310 , , TPS62130 , TPS62813M , TPS62813-Q1 Tool/software: Hi team,
My customer is considering the TPS54310 because it is used in the TMS320C6713B EVM. However, I'm concerned that it is…
Part Number: TMS320C6713B In the application of interest, the application program code is copied from external nonvolatile memory into the DSP internal RAM when power is applied. Operation from internal RAM supports fast operation. To verify a correct…
Part Number: TMS320C6713B Tool/software: I am considering the TMS32C6713BGDPA200, but I believe it is an older device. Are there any newer DSP devices equivalent to the TMS32C6713BGDPA200?
Part Number: TMS320C6713B Out existing product was built on Code Composer 5.2. I am now tryinfg to update to 12.7...
When I try to build I get:
This project's device is not supported by compiler version 8.3.2: ( should I be using a different version…