Part Number: TMS320C6746 Other Parts Discussed in Thread: OMAPL138
Hello. I would like the source code for the TMS320C6746 bootloader. Can I obtain it?
Part Number: TMS320C6746
Hello everyone.
I am trying to "NOR BOOT" the FW of my "TMS320C6740".
If the FW is within 16KB in size, I can boot it in "Legacy NOR Boot" mode.
However, the FW that I really want to use is over…
Part Number: TMS320C6746 Dear Tii,
can anyone please guide me how to program .out file from CCS to the TMS320C6746 external NAND flash and boot from it,
i have read about AISgen for D800K008, that takes ELFFor COFF files and genrerate AIS image, is there…
Yes, you can load code into DSP C674x L2 RAM as long as L2 RAM has been configured to not act as cache. Explicitly set the L2 RAM as 0 cache in the DSP configuration registers.
0x0080 0000 0x0083 FFFF is the local address of the DSP L2 RAM and 0x1180 0000…
Part Number: TMS320C6746
Hi,
I have following queries:
1. Whenever I read the receive buffer (RBUF) using interrupt/pooling, it reads 0 or all F's; in scope but I see different data. My question is, what could cause the data in scope and in RX register…
Part Number: TMS320C6746 Other Parts Discussed in Thread: OMAP-L138 , OMAPL138
Dear Support:
We are using custom board which has TMS320C6746 DSP. I am looking for bare-metal (Non-OS) McBSP driver for this DSP. Can you please direct me where I can get it…
Part Number: TMS320C6746 Other Parts Discussed in Thread: OMAP-L138 Hi,
We are using custom board which has TMS320C6746 DSP. I am trying to use Digital loop back (DLB) mode which allows the testing of serial port code without using the external interface…
Part Number: TMS320C6746 Hi Experts,
Seeking your assistance in this query please:
Would like to confirm of these highlighted parameters. What are they representing for?
Thanks ahead for your detailed response.
Regards, Archie A.
Part Number: TMS320C6746 Dear TI,
I have to calculate HPI bus timings, below timings from TMS320C6746 datasheet page196
For timing No. 4 i.e. tw(HSTBH) = 2M, it is written that M=SYSCLK2 period in ns
at page 87 of datasheet SYSCLK2 is given, but there…