Part Number: TMS320C6746 Hi Experts,
Seeking your assistance in this query please:
Would like to confirm of these highlighted parameters. What are they representing for?
Thanks ahead for your detailed response.
Regards, Archie A.
Part Number: TMS320C6746 Hi team,
In the datasheet, there are requirements for the OSCIN.
For tw(OSCINH) and tw(OSCINL), it says the min is "0.4 tc(OSCIN)".
Is this applicable for all the f_OSCIN range? (The customer is going to use 24.576MHz…
Part Number: TMS320C6746 Hi,
I am looking for the information about HPI bus electrical parameters like setup time, hold time etc. for signals like UHPI_CS, UHPI_HDS1, UHPI_HDS2, UHPI_HR/W etc. Kindly guide towards the correct technical literature.
Regards…
Part Number: TMS320C6746
Dear TI,
We are planning to use HPI bus of TMS320C6746 as below
- there will be two boards based on TMS320C6746 processor, and we will connect HPI bus of these two TMS320C6746 processors in parallel,
and a third master processor…
Part Number: TMS320C6746 Dear TI,
our query is as below
- As written in TMS320C6746 documentation that external Host processor can access all interna and external memories over HPI bus,
In our case, we have connected external DDR2 memory to TMS320C6746…
Part Number: TMS320C6746 Dear TI,
i) can you pls. help to get utility serial flashing mentioned in this post
TMS320C6742: Serial Flashing Host Utility sfh_OMAP-L138 usage for C6742 DSP - Processors forum - Processors - TI E2E support forums
may you send…
Part Number: TMS320C6746 Dears,
Does emu0 emu1 pin have to be pulled up, customer left it floating, unable to burn the firmware; the log as attachment.
24885.LOG.txt
[Start: Texas Instruments XDS100v2 USB Debug Probe_0]
Execute the command…
Part Number: TMS320C6746 Hi,
In Processor datasheet under the unused pin configuration the RTC_XI pin suggested to connect high or low if RTC section not used..
Will it have any impact if the RTC_XI pin left as floating/No Connect? Please confirm.
…