Part Number: TMS320C6748 Dear TI Technical Support Team,
We would like to know what will be state of the below GPIO pins of TMS320C6748EZWTA3 when Processor is in reset state.
1) GP3[9] [Pin - D10] 2) GP6[3] [Pin - K3] 3) GP6[1] [Pin - K4]
Regards…
Part Number: TMS320C6748 Hi experts,
Is it possible to realise the following configuration using the uPP (Universal Parallel Port) of the C6748?
Prepare three DSPs and connect them as shown in the diagram below.
DSP0 sends the same data to DSP1…
Part Number: TMS320C6748 Other Parts Discussed in Thread: OMAP-L138 Hi Expert,
I am posting this on behalf of the customer. Here is the inquiry below.
I am unable to get the expected result. I am actually trying to get a sinewave output at the Lineout…
Part Number: TMS320C6748 I have a TIRTOS system with just two tasks: and audio processing task and a SPI comms task using SPI 1 configured in 4-pin mode using SPI1_SCSn_0 pin. SPI1 is basically not working as advertised.
Summary of my findings:
…
Part Number: TMS320C6748
Hi,
Good Day.
I have a customized board with c6748 and I want to boot from 16-bit width NOR flash.
I've seen a little bit of the NAND bootloader of the reference board and starter wear, but NOR has not found the bootloader…
Part Number: TMS320C6748 HI,
I have a DMA for McASP TX setup which is running in sync with the McASP clocks but there is no output..
If I hard code writing to MCASP_DMABUF for all enabled outputs all outputs are good all of the way through to
producing…
Part Number: TMS320C6748 Hi,
We use TMS320C6748EZCEA3 that has 75,000POH.And it is almost used with deep sleep condition. I want to know if POH includes of DEEPSLEEP condition.
regards, Keitaro Nakagawara
Part Number: TMS320C6748 Other Parts Discussed in Thread: BQ25890
Hi,
The chip I used in our product is TMS320C6748EZWTD4.
The CPU freq and DDR freq are both set at 80MHz.
RVDD is set as 1.2V.
When CVDD is 1.2V, everything runs OK. Our product…