Dear All,
I use virtual box software and ubuntu 16.04 to develop my project.
I copy mvl_4_0_1_demo_sys_setuplinux.bin to /davinci folder.
I type "./mvl_4_0_1_demo_sys_setuplinux.bin" in /davinci folder but I can't find mvltools4.0.1-no-target.tar…
Hi David,
Interrupt number 18 is shared between SPI1_INT1 and EDMA_TC0_ERR_INT. So, either one of the interrupt can work at any give point of time. However, you can stil use EDMA module without configuring TC0_ERR_INT [With some compromise].
Th…
Hi,
I hope above inputs were helpful in solving your issue.
If the issue is resolved then please close the thread by verifying answer.
Regards,
Anuj
Pathpartner Technology Pvt Ltd
Hello,
What you mean?
Could you provide more details.
Please check this guides also:
processors.wiki.ti.com/.../GSG:_Running_the_DVEVM_Demos
processors.wiki.ti.com/.../DM3xx_integrate_new_codec_in_DVSDK_3.10
BR
Margarita
Part Number: TMS320DM355 Tool/software: Linux
Need to modify the SpiDev / Davinci_Spi.c to support "Waiting" for a Signal from DRDY from an ADC (Specifically the ADC1278) so that we only start reading once we have DRDY signal confirming that data is…
Figured this out - the streams created are Elementary streams and need to be converted before they can be played through a commercial player such as WMP or yes, even VLC.
All good. :)
Other Parts Discussed in Thread: TMS320DM355 Dear All,
I am just wondering to know if it is possible to use (TMS320DM355 evaluation board) with MS-Windows? in the datasheet it seems it can be used with Linux.
Any one have used this device before…