Part Number: TMS320DM365 Hi,
Please let me know what is minimum time delay required between various rail TMS320DM365 ie between 1.35V, 1.8V and 3.3V rail and what should be sequence
Part Number: TMS320DM365 Tool/software: Linux Hi,
Our customer is using JPEG encoder 01.00.00.12. software-dl.ti.com/.../index_FDS.html
The release notes have the following description. SDOCM00091259 Bottom Row corruption when image height is non multiple…
Hi,
Support for this device is very limited, for any detailed software or hardware support, bug fixes, or enhancements to the software, please contact the partners recommended below. They have extensive software expertise and systems experience. Customers…
Part Number: TMS320DM365 Other Parts Discussed in Thread: TVP5158
Tool/software: Linux
Hi all, Refer to TVP5158 datasheet, as figure below shows, in pixel-interleaved mode, all channel data will interleave together, include SAV/EAV code, so obviously…
Part Number: TMS320DM365 Hello,
Now, I'm considering how to output WVGA LCD display from TMS320DM365. LCD is parallel RGB666 and pixel clock must be higher than 30.3MHz.
For above conditions, I have two questions.
1. In case DM365-216, the maximum…
Part Number: TMS320DM365 Hi TI !
I am using KIT tms320dm365 evm to develop a DVR device.
I want output digital video YUV422 8Bit over port J18 vs J19 in KIT EVM to display in OLED screen.
Please tell me the way to do it.
I using dvsdk_dm365-evm_4_02_00_06…
Part Number: TMS320DM365 Hello,
I think that the library included in DVSDK is compiled by gcc v4.3.3. Could you release recompiled DVSDK by gcc over v4.8? My customer wants to use application which is compiled by gcc4.8; therefore, it seems that the coherence…
Part Number: TMS320DM365 Tool/software: Linux Hi, Can anyone provide me with a starting point for using Arago with the DM365 SoC? I would like to use this to make my rootfs.
Thanks,
Doug Burrell
Part Number: TMS320DM365 Tool/software: Linux I need some advice on the TMX320DM365 evaluation board as I used it many years ago but need a quick answer now whether it is possible to use the input video as NTSC at 60Hz and convert it to the output of PAL…
Part Number: TMS320DM365 Hi,
Is there any plans to make the part: TMS320DM365ZCED30 obsolete?
Please let me know when would be the expected date if any plans for the same.
Thanks & Regards,
Nanjunda M