Part Number: TMS320DM6437 In the tech reference manual of DM6437 it was given that, DDR2 memory is 128 MEGABYTE.There are two DDR2 memories .So, each having 128 megabyte capacity or combination of two having 128 megabyte capacity?
Hi Sai,
A phase-locked loop or phase lock loop abbreviated as PLL is a control system that generates an output signal whose phase is related to the phase of an input signal.
For general PLL concept explanation, refer to the below links:
en.wikipedia…
Part Number: TMS320DM6437 Hello,
I have tested the DM6437 with a normal camera with NTSC/PAL output & it works great.
Now i just need to know the following
1) what and all camera modules(specifications) it can support,does it support any one…
Enhancement request SDSCM00043204 "Copy user supplied binary file directly into the output executable" was raised in response to the previous thread placing binary resources in the linked executable . However, SDSCM00043204 has not yet been implemented…
Part Number: TMS320DM6437 Hi everyone,
Am generating C code for normal DIPswitch LED and videocapture and Display using Matlab2012b Simulinkmodel with CCSv3.3 for DM6437 kit, code generation building loading program to target everything will done perfectly…