Part Number: TMS320DM8127 Tool/software: Linux Hi,
Our Customer is using the Device : DM8127, SDK : IPNCSDK_3.8.0 and Linux version 2.6
Our issue is a late time out of bad sd card.
So we reviewed the omap_hsmmc.c(mmc driver) of Linux version 2.6 for DM8127…
Part Number: TMS320DM8127 Tool/software: TI C/C++ Compiler In the TMS320DM8127 data sheet section 3.12 Memory Map Summary the tables 3.5 and 3.6 make reference to Peripheral and Support registers. What is the difference between these two sets of registers…
Part Number: TMS320DM8127 Tool/software: TI C/C++ Compiler I am trying to program the TMS320DM8127 interrupt controller INTC using the Table 14-3 of the SPRUGZ8G–14 Technical Reference document which lists the various registers within the INTC. …
Part Number: TMS320DM8127
Tool/software: Linux
Good day, experts. I need your help. I have camera starter kit with DM8127 procesor andAR0331 Leopard camera sensor (was included to kit). I use preformatted SD which came with kit to boot linux and streaming…
Part Number: TMS320DM8127 I use this device to do some video compression and decompression , by connect the DPS with FPGA ,which pins should I use in this design ? the GPMC pins are connected,any other pins should use?
Part Number: TMS320DM8127 Hi,all
I add a new sensor mt9v034(752x480) on dm8127 platform.After configure mt9v034,it can only capture about 60 frames,then the system abort.how does it happen?
My sdk is ipnc_rdk 3.8.Below are moficaitons:
ISIF:
isifCfg…
Part Number: TMS320DM8127 HI
The TMS320DM8127 Digital Media Processor is said to support the AR0331 ROLLING SHUTTER CMOS Sensor.
I want to use Global Shutter CMOS Sensor instead of ROLLING SHUTTER CMOS Sensor.
Do you support Global Shutter CMOS Sensor…
Part Number: TMS320DM8127 Other Parts Discussed in Thread: TMS320DM8148 Hi,
We need video processor to recognize BT.656, have any TI solution can support it.
Warm Regards,
Lin
Part Number: TMS320DM8127 Hi - I'm trying to configure 4 pins of GPIO 0 on the DM8127 as outputs, The software performing the configuration is C code running on the DSP core. The GPIO registers when viewed in a CCS memory window are all 0-valued - even…
Part Number: TMS320DM8127 Tool/software: TI C/C++ Compiler I am trying to write a C application for the TMS320DM8127 using the TI ARM compiler within CCS8.0
Could you tell me if there are any header files that contain all of the internal device specific…