Part Number: TMS320DM8147 Other Parts Discussed in Thread: CCSTUDIO
Hy everyone,
We just received our pre-flashed nand (Spansion S34ML02G100BHI1000) for our custom board....which however won't boot.
As I assumed there is something wrong with the ECC…
Part Number: TMS320DM8147 I have a situation where EDMA3 transfers to/from McASP works fine at 96 kHz, but when I increase the sample rate to 192kHz the are occasional (every 2-3 second) very small audio glitches.
There are other transfers using EDMA…
Part Number: TMS320DM8147 Other Parts Discussed in Thread: CCSTUDIO Tool/software: TI-RTOS
Hi,
I am using third party phy on TMS320DM814 based customised board.
Ethernet is configured over SPI rather than mdio on the board.Are there any registers related…
Part Number: TMS320DM8147 Tool/software: Linux Hello,
We are planning to connect a TVP chip (which multiplexes 4 Analog video inputs PAL/NTSC) to a single Video Input port (8 bits) of DM814X.
From my understanding, DM814X video input port is capable of…
Part Number: TMS320DM8147 Other Parts Discussed in Thread: SPRC121 We're using the 8147 processor, and are trying to do some signal processing. The TI FFT and BitReverse C routines come from:
TMS320C67x DSP Library Programmer’s Reference Guide…
Part Number: TMS320DM8147 Tool/software: Linux dears,
now the DM8147 as a slave, the PCIE of DM8147 communicate with intel X86,the problem we accros is the driver run on Linux. as we discussed with the Intel, the driver can acquired from you. so how can…
Part Number: TMS320DM8147
Tool/software: TI-RTOS
PC net configuration: IP =192.168.1.10, Mask=255.255.0.0, DaVinci Device IP =192.168.0.250, Mask=255.255.255.0
The NDK stack of the device replies to Ping from PC, although the PC is not in the same subnet…
Other Parts Discussed in Thread: TMS320DM8147
Customer planning on using TMS320DM8147 when available. looking for the staus on the following API called
"calib3d," and in particular a function
"cv::StereoSGBM::operator ()" that we would need…
Hi Connie,
The DM8147 and DM8127 are very similar parts but they differ in capability based on the availability of GPU, Face Detect IP, differences in the capability of the ISP block and also peripheral mix that is supported.
To get to the exact details…
Hello,
Please refer to the DDR2 Signal Termination section of the device datasheet for details on termination requirements. In general, pay close attention to the details in the DDR2 Routing Guidelines section.
Regards, Marc