Part Number: TMS320DM8168 Hi,
In our board currently the DDR3 density support/ we are using is 1GB by making use of the DDR0 controller connected to 4 x 8bit DDR3 chips, each with density of 256MB (256MB x 4 = 1GB). We would like to confirm if we…
Part Number: TMS320DM8168 Tool/software: We are Re-evaluating the PCB routing of a system based on TMS320DM8168CCYGA2 and need to understand the length matching constraints required for GMII TX and RX pairs as well as any specific layout guideline is…
Part Number: TMS320DM8168 Hi,
This is regarding SD card Write issue in one of the multiple boards ( https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1295197/tms320dm8168-query-regarding-sd-card-issue/4916417#4916417 ).
I just…
Part Number: TMS320DM8168 Other Parts Discussed in Thread: TVP5150 Hello...!
Good day.
We are testing the TMS320DM8168CCYGA2 processor for recording purpose and it should work under the Ambient Conditions of 72°C.
Construction :
We have customized…
Part Number: TMS320DM8168 Other Parts Discussed in Thread: TMDSEMU200-U Hello all,
I'm looking to better understand what probes and tools I need to properly debug a kernel loading bug on the TMS320 DSP. I work on the hardware side and have extremely…
Part Number: TMS320DM8168
Hi,
We are using TMS320DM8168CCYGA2 in our design since past 8+ years. The boards are already under production since many years.
In one board we are facing an issue w.r.t SD card write. The write is failing with echo commands…
Part Number: TMS320DM8168 Hi, We are looking for supporting two video Capture inputs simultaneously - VIN[0] as 24-bit and VIN[1] as 16-bit. As per the datasheet support is available for the same.
But on checking the IOMUXing of these interfaces,…
Part Number: TMS320DM8168
Dear Support Team,
My name is Bandar, and I am currently working on a research project involving processor DM8168. I have been trying to locate the reference design for product DM8168, but unfortunately, it seems to be…
Part Number: TMS320DM8168 For an ongoing project we are currently using a camera which uses 5V UART transmission. As per our customer requirement we are switching to a camera which uses 3.3V UART transmission. We are using TMS320DM8168 as the microprocessor…
Part Number: TMS320DM8168 Hello
Our application is a kind of DVR and we developed that product using TMS320DM8168 through DVRRDK.
The simple description of our product is as below.
Download various videos from IPCAM and decode CAM images. Then show…