Part Number: TMS320F280025C-Q1
Hi Champs,
I know that GPIO12 and 13 are assigned to flash test pins for F28004x PMQ package. So, users can't use these two pins in a 64-pin Q-100 device. I'd like to know whether F28002x is also the same situation or…
Part Number: TMS320F280025C-Q1 Other Parts Discussed in Thread: UNIFLASH Hello support team,
I have 2 SW (2 hex files):
- SW1: custom bootloader with entry point 0x80000
- SW2: application with entry point 0x84000 (or 0x83000)
I want the boot…
Part Number: TMS320F280025C-Q1 Hello support team,
I have 2K*16 in GS0 Ram but it's not enough for our application
I tried to use RAMLS4567 instead:
28002x_launchxl_demo_flash_lnk.cmd:
SECTIONS
{
codestart : > BEGIN, ALIGN(8)
.text : >> FLASH_BANK0_SEC2…
Part Number: TMS320F280025C-Q1 Other Parts Discussed in Thread: C2000WARE
Hello support team,
I have a custom bootloader SW at flash sector 0-2.
After doing some tasks I want to jump to an application SW at flash sector 3-7 (same BANK0) without…
Part Number: TMS320F280025C-Q1 Hello,
I'm Alex. Kim from south Korea.
I'm wondering about CAN Stack with J1939 and UDS on TMS320F28002x.
My customer request me to implement a CAN Stack with J1939 and UDS for MAN Truck.
But We don't have any experience…
Part Number: TMS320F280025C-Q1
Hello support team,
I can read the ADC result with DMA, then I'd like to read the status of GPIO pins.
But when I replace the DMA source "&AdcaResultRegs.ADCRESULT0" with "&GpioDataReadRegs.GPADAT_R" or "&GpioDataRegs…
Part Number: TMS320F280025C Tool/software: Hi there,
I have been successfully sending and receiving CAN by calling my CAN_receive_routine() and CAN_send_routine() in my main loop. The CAN_send_routine() simply contains a bunch of CAN_sendMessage(…
Part Number: TMS320F280025C Other Parts Discussed in Thread: DRV8323 , BOOSTXL-DRV8323RH , BOOSTXL-DRV8323RS Hi, I encountered the following issues in my incremental build project with F280025C+DRV8323RH.I hope you can answer it for me.
Q1:A ccording…
Part Number: TIDA-010236 Other Parts Discussed in Thread: TIDA-010203 , TMS320F280025C Tool/software: Hi,
I am looking for a totem pole PFC solution with TI products.
[Conditions]
- Input voltage: AC200V or 400V
- PFC output: 400V
- Output power…
Part Number: TCAN1145EVM Other Parts Discussed in Thread: TMS320F280025C , TCAN1145-Q1 , USB2ANY We are using TCAN1145-Q1 along with TI DSP TMS320F280025C. We want the sample code for the same. From where can we get sample code to configure TCAN IC using…