Part Number: TMS320F28052 Tool/software: I have a question regarding the operation of the C2000 series built-in I2C module. Currently, in I2C Master Write mode, we are sending "address + 2 bytes of data" to an LCD device. However, when sending the address…
Part Number: TMS320F28052 Hi, I have an issue with my debbuger, an XDS110 debug probe connecting to the F28052 micro-controller.
I am able to connect to the micro and flash the program into it, but whenever I enable the micro to begin running an applicaton…
Part Number: TMS320F28052 Tool/software: Immediately after debugging “C28xx: Trouble Setting Breakpoint with the Action "Finish Auto Run" at 0x3f2711: (Error -1066 @ 0x3F2711) Unable to set/clear requested breakpoint. Verify that the breakpoint address…
Part Number: TMS320F28052 Hi,
1) Is it okay if the yellow pins are open when JTAG is not connected?
2) Is the following how to handle unused pins?
GPIO ・ ・ ・ Open and set to "output"
3) Are there any requirements other than the following regarding…
Part Number: TMS320F28052M Other Parts Discussed in Thread: DESIGNDRIVE Hi,
What is the suggested upgrade path for our drive design to support an absolute position feedback sensor, such as HIPERFACE, SIN/COS, HIPERFACE DSL, etc?
We current use the…
Other Parts Discussed in Thread: TMS320F28052 Re: TMS320F28052 Analog Port Injection Current
I need to know how much analog input injection current, over the uP's temperature range, will start to affect adjacent/other A/D inputs.
This isn't a normal…
TMS320F280049C will not support InstaSPIN Motion. The only device we support InstaSPIN Motion will be TMS320F28068/9M and TMS320F28052/4M. For more details, please refer to https://www.ti.com/microcontrollers/c2000-real-time-control-mcus/applications…
Part Number: TMS320F28386D Other Parts Discussed in Thread: C2000WARE Hi C2000 Champ !
As I checked the availability via C2000-IEC60730-SW-PACKAGE page. I am not able to find TMS320F28386x device in the list.
Can you please clarify if TMS320F28386x…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Hi Craig,
If you are looking for boot to flash, please refer to this similar thread first: How to boot F28069 from internal flash
and this: /cfs-file/__key/communityserver-discussions-components-files/171/3618.Running-from-Internal-Flash.pdf
Best…