Other Parts Discussed in Thread: TMS320VC5401 Hello
I'm working on an audio related project. I have to send a sample to the DAC of my board every 48kHz. The sending is OK as I have written a small code to write to it (two channels). Now I have to…
Hi all.
How can I access (set and reset) the XF pin in C using CCSv5? I have installed the CSP libraries but I could found any references to it.
Thank you.
Other Parts Discussed in Thread: TMS320VC5401 Hi,
I want to use external RAM in my program.
But i am not able to access it, if i run program from Internal memory then program is working fine.
and if i try to run program from EXTRAM then DSP…
Other Parts Discussed in Thread: TMS320VC5401 , TMS320VC5505 Hi,
After working on TMS320VC5505 now i am working on TMS320VC5401.
But during this development i am facing some problems,
Generally in 5505 to access the peripheral registers (like…
Other Parts Discussed in Thread: TMS320VC5401 For the first time, I use a TMS320VC5401 to design an audio amplifier along with an ADC and a DAC. Say the sample rate is 48KHz (typically for audio processor), how do I choose a value of the external crystal…
Part Number: PCM1754 Other Parts Discussed in Thread: PCM1808 , TMS320VC5401 ,
Dear TI FAE,
I'm working on a project using PCM1808 and PCM1754. Partial schematics and layout below. The goal is to replace an existing codec with these ADC and DAC…
Other Parts Discussed in Thread: TMS320VC5401 Hi all.
I'm trying to get used to the TMS320VC5401 DSP. I'm trying to write a simple program: to read a sample from the sine table and write it to a external device using PORTW instruction. The question…
Support Guidance for C55x, C54x, C5x
Q: I’m developing an application based on TI’s C5000 family of digital signal processors. I have some questions and need some support. Can you help me?
A: Thanks for reaching out.
Links to active C5000 devices…
Other Parts Discussed in Thread: TMS320VC5401 Hi All,
is it possible to perform floating point calculation using CCSV4 for TMS320VC5401 processor?
Thanks & Regards,
Ashwin Panchal