Part Number: TMS320VC5505 Tool/software: Code Composer Studio Hi All,
I am using evaluation board TMDX5505eZDSP (TMS320VC5505). I have used I2C bus and CSL library with this board successfully in the past.
Currently I am working on the project which requires…
Part Number: TAC5112EVM-K Other Parts Discussed in Thread: TAC5112 Tool/software: Hi, I'm trying to drive TAC5112EVM(as Target mode) by TMS320VC5505-USBSTICK-EVM(Of course without AC-MB). And primary, I'm going to try DAC out with PASI_TX_CH0 by sending…
Hi Yutaro,
The only differences between the C5505 and C5504 are 64KB extra on-chip memory, HW FFT, Integrated LCD display controller and 10-bit 4-channel SAR ADC.
You can get the C5505 DS from: https://www.ti.com/lit/gpn/tms320vc5505
Best regards,
Min…
Part Number: TMS320VC5505 Other Parts Discussed in Thread: TMS320C5505 , Hello,
Do you have a migration guide for VC5505 to C5505?
Before, there was a link at below thread.
https://e2e.ti.com/support/processors/f/791/p/40360/1450628
But I can get it no…
Part Number: TMS320VC5505 Tool/software: Code Composer Studio Hi All,
I have been evaluating TMS320VC5505 using TMDX5505eZDSP evaluation board and Code Composer Studio. The evaluation was going very well I created project based on DSP/BIOS I could load…
Part Number: TMS320VC5505 Other Parts Discussed in Thread: TMS320C5504
Hello,
My customer needs to estimate the maximum value of the CVDD current. A sample value would be accepted. Could you please advise?
Condition: * 1.3V * Processing at Full load. * …
Part Number: TMS320VC5505 Hello, Do you conern if the total current consumption of 3.3V supply differs 12mA part-to-part? Or do you expect a larger deviation of that?
Customer test result:
Device# Lot# Current consumption, 3.3V total [mA] 1 47AGPSW 129 …
Part Number: TMS320VC5505 Is there an optimized CRC calcuation routine for the G.722.2 IF1 CRC? The encoder calculates the CRC and outputs it correctly. The RX/decoder side must calculate the CRC of the ClassA bits and compare it to know how to call the…
Part Number: TMS320VC5505
Tool/software: Code Composer Studio
Dear All,
I am using circuit board of TMS320VC5505 eZDSP USB STICK (Revision B) and information on it can be found at support.spectrumdigital.com/.../ .
I downloaded CCSv4 from http…
Part Number: TMS320VC5505 Hi,
I recently wrote a simple software for the TMS320VC5505 eZdsp Stick (revB) by using the usual example code . Everything was working fine until I loaded the program to EEPROM using the eZdsp Programming Tool (programmer_USBKey…