Other Parts Discussed in Thread: TMS320VC5505 Hi all
I'm trying to open the Layout Info for the TMS320VC5505 eZDSP USB STICK (Revision C) avaliable on:
http://support.spectrumdigital.com/boards/usbstk5505/revc/
I tried with Eagle and I get an…
Other Parts Discussed in Thread: TMS320VC5505 Hi,
I have a 40-bit function which was created and compiled on a PC in a C environment.
I need to compile and run the function on the TMS320VC5505 DSP chip in a CCS4 environmet.
The problem is that the…
Other Parts Discussed in Thread: TMS320VC5505 , TMS320C5515 Hi I work on the TMS320VC5505 and I want to use the SAR to measure the battery's voltage. I have done it without use CSL. I use the channel1. And I don't understand the value in SARDATA. For…
Greetings, i am wondering if you could help me (it would mean a lot to me). This is code i wrote for CCS... #include "stdio.h" typedef volatile unsigned int REG; #define REG1 ((REG *) 0x00000003) void main (void){ unsigned int i=0, delay = 100; while…
Hi,
I have spent almost 3-4 weeks to get properly init the timer0 interrupt,
The interrupt examples,user guides given by TI is create more confusion and also it eat our time.
The attached example code is simple, in this example the Timer-0 is initialized…
Other Parts Discussed in Thread: TMS320VC5505 Hai,
I am using TMS320VC5505 EVM , I want to interface PulseOx MDK with that, The CD comes along with the PulseOx MDK th codes in that is working but with some warnings, As a result i cant able to get the…
Other Parts Discussed in Thread: TMS320VC5505 Hi,
Is there an external memory card available for use with TMS320VC5505? Any pointers on this will be useful.
Thanks
Abhishek Seth
Other Parts Discussed in Thread: TMS320VC5505 I have found a problem about I2S and DMA when I used them on my evaluation board(TMS320VC5505). The problem is described as follows:
Set I2S2 left channel transmit and receive in Loopback Mode. Use CSL_DMA_CHAN6…
Other Parts Discussed in Thread: TMS320VC5505 I am putting the TMS320vc5505 on a board, it says on the product page it has a UART. In the datasheet it says it has a UART, but also in the datasheet on page 60 section 6.4.2 it says:
UART is currently not…