Hello again,
after some try outs with my EVM I tried to implement a own ring buffer FIR in C like this example:
http://www.fh-schmalkalden.de/schmalkaldenmedia/Realisierung_Digitaler_Filter_in_C.pdf
I use Q15 coefficients placed in the DARAM. But…
Have migrated to csl 2.0, built all projects, updated dsl/bios.
All the builds were ok.
What Target Configuation do I use
Dont have the options as before under csl 1.0.
Martin
I installed CCS V4.0.0.16000 on Vista 64-bit machine and plugged in the eZDSP. Vista didn't recognize and tried to install the driver. I inserted the disc and it still couldn't install the driver. I did CCS software update uninstall/reinstall the driver…
Hi,
I have 2 questions on ECG daughter card for VC5505.
1. J22 is a 2x11 double row male header on VC5505 EVM which is used to interface the ECG front end daughter card and VC5505 EVM. But the corresponding female on the daughter card is 2x10. I have…
Hello,
I tried to configure Profiling like described here:
http://processors.wiki.ti.com/index.php/Profiler
But I have the problem that the processor runs at ultra low speed after activating the profiling functions
Does somebody have an idea or is…
Other Parts Discussed in Thread: SPRC133
Hi All,
Can anybody let me know how to create timer interrupt (In CCS-V4, using C) without using any DSP library and DSP BIOS?
I also read out "SPRA036" but it create more confusion.
Thanks in Advance…
Hi, Srinivasan,
I don't see anyone in the TI directory with that name.
I suggest you try posting in the MSP430 forum, they will either help you, or point you to the correct place for help.
-d2
Other Parts Discussed in Thread: TMS320VC5505 I'm trying to getting started with the TMS320VC5505 ezDSP USB Stick but I'm very new and I'm having some problems in enabling CCS v4 to use CSL and in finding libraries and make them work correctly. In particular…
Other Parts Discussed in Thread: TMS320VC5505 I am trying to save acquired sensor data from the Pulse Oximeter TMS320VC5505 DSP Medical Development Kit (MDK) to the onboard SD card, so I thought I would start with the TI CSL examples. All of the mmc_sd…
Hi Adnan,
Thanks for the post.
You will not be able to use the suggested Olimex cable with the ADS1293EVM directly. Some vendors (see links below) sell the ECG cable for the ADS1292 EVM with a similar DB9 connector. However, this cable only has four electrodes…