Hi Ramesh,
I talked to my colleague today. Here are a few things you can do:
1. In C5509A DSK, there is a dip switch S3-1 to control the value of GP0
Which in turn determines the A0-13 used for HPI or EMIF. Make sure it is used for EMIF addressing on…
Part Number: TMS320VC5509A Hello Experts,
I need to ask you about the TMS320VC5509AZAYR.
When using 128Mbit (8Mx16) SDRAM, according to the Reference Guide below, cs[3:1] should be left unconnected using CE0 only. https://www.ti.com/jp/lit/ug/spru670a…
Part Number: TMS320VC5509A Hi Experts,
Our equipment uses TMS320VC5509A and we are experiencing problems with this equipment. The problem is that the McBSP output signal has jitter. As an investigation, I configured the CLKOUT pin to output CPU CLOCK. As…
Part Number: TMS320VC5509A Hi Experts,
Please tell me about the relationship between CLKIN and McBSP output clock(CLKX) in TMS320VC5509A. CPU CLOCK is generated by multiplying CLKIN by 4 using the internal PLL. McBSP's output clock (CLKX) is generated by…
Part Number: TMS320VC5509A Other Parts Discussed in Thread: TMDSCNCD263P I have cards that many times the cards stop working, when I check them I see the VCC_ALOG (AVdd & ADVdd) is shorted to GND.
When we replace the DSP TMS320VC5509A, the problem…
Part Number: TMS320VC5509A Hi, all;
This is Masayuki and I'm supporting DSP customers.
We found SPRS163F Reference Guide described for the 12MHz crystal for TMS320VC5509, TI is recommended to use lower one of MAX ESR 40 Ohms.
Our customer is in stock…
Part Number: TMS320VC5509A For this chip TMS320VC5509APGE, is there a suitable recommendation for the input software and programmer? We used Hyperterminal to write it, but there was a problem
Hi Aditya,
Attached please find the A-law codec in C#. You should be able to find out the value to initalize vocoder for 0xD5.
Best regards,
Ming
----------------------------------- Cut Here ------------------------------------------
A-law Encoding
A-law…
Hello,
Software is not working, If I define the extern variables in a particular file (ex. main.c) but it works If I define the same variable in different file (ex: test.c). Also if I initialize with 0 its not working but If I initialize with particular…
Part Number: TMS320VC5509A Hi Team,
Here's an issue from the customer may need your help:
Self-built project import files encounter assembly file error reporting:
Statements in comments are also compiled as errors.
Some of the assembly instructions…