Part Number: TMS320VC5509A Hello, My customer would like to know the Internal Pull-Up and Pull-Down resistor value as follows. Q1: How much ohms (min/max) is the internal Pull-Down resistor at TRST pin? Q2: How much ohms (min/max) is the internal Pull…
Part Number: TMS320VC5509A I want to use USB peripheral for TMS320VC5509A to communicate with a USB host. I am using C55xx CSL (Chip Support Library) version 2.31.00.9 to initialize USB module and USB communication. I have read documents titled SPRU433J…
Part Number: TMS320VC5509A Hi,
I have a TMS320VC5509A and I want to update a new application code via USB. I created boot table (binary file format) from object output file using hex55 tool "SdrBios.out --boot -v5509A -serial8 -reg_config 0x1C00…
Part Number: TMS320VC5509A Hi Team,
Could you tell me the maximum current consumption (ICC) of the USBPLLVDD? I checked spraa04a.xls and there is no mention of USBPLLVDD.
Best regards, yoshi.Y
Part Number: TMS320VC5509A Hi Experts,
Our customer developed their system with TMS320VC5509APGE and they are releasing this system in the market for a long time. Recently, customer noticed there is a symptom that part of program which was stored in DPS…
Part Number: TMS320VC5509A Hi Team,
Recently I configured Mcbsp0 as a spi slave, and the relevant register configuration is as follows. (I referred to Section 6.7 of SPRU592E.) The code comment is not accurate, and the DSP receives data on the falling…
Hi Peter,
Peter Campbell said: To capture the fail scenario, I'm heating the DSP up to around 50C. At room temp, it passes every time. Warmed up, it fails consistently.
Thanks for sharing this additional information. The seems like an important observation…
vikas negi1 said: Any interrupt/power failure during update should not effect the booting process.
It's not possible for a power failuire to not affect boot or run-time behavior of the device.
vikas negi1 said: And in next power ON also fresh attempt…
Hi Maynard,
I was able to locate this guide on an archived wiki page. According to this guide, the C5507 and C5509A have the same CPU revision 2.2.
C55x_CPU_revision.pdf
Regards, Frank