Part Number: TMS320VC5510A Tool/software: Datasheet for part number TMS320VC5510AGBCA2 calls out the ZGW and GGW packages instead of the GBC package (which is linked separately).
Is the datasheet in error or is there some equivalance between the two packages…
Hi Shao,
The only other feedback I got is to check if this link provides any further information that is useful: https://software-dl.ti.com/dsps/dsps_registered_sw/sdo_sb/targetcontent/bios/bios_5_20/sabios-e23/docs/SetupGuide.html
Beyond that, we do not…
Part Number: TMS320VC5510A Hi TI Support,
I am migrating my older CCS project which are based 3.3 which were based in XP to latest CCS version. But I need to migrate them in stages by first going to CCS 6.2 which was the last version for XP. When I get…
Part Number: TMS320VC5510A Hello everyone,
I used ccs2.2 to build one project once before, and the .out file worked successfully on my chip with no error;
However, when I try to use ccs7.4 to rebuild the same project (nothing changed), the .out file couldn…
Part Number: TMS320VC5510A Hello everyone,
I have met several problems while using the ccs。
I use ccs2.2 to compile my previous project,no error。However,when it changed to ccs7.4,it showed error #10099-D。Therefore,what can I do in order to solve this…
Part Number: TMS320VC5510A Hi Experts ,
Please refer to below image of BGA Component and confirm me it is under acceptable level or not?
Please let me know acceptable criteria for BGA components.
Looking for your valuable support.
Regards
Manoj Balakrishnan…
Part Number: TMS320VC5510A We are developing an application for the TMS320VC5510A chip where we are loading the program from an external flash. The process to do so involves reading the program data from the flash and parsing it according to the boot…
Other Parts Discussed in Thread: TMS320VC5510A , TMDSEMU200-U I am trying to load a program in code composer 12.3 to a TMS320VC5510A chip. I am using the TMDSEMU200-U Debug probe as a connection. In the target configuration options there is no option for…