Hello.
I am working on a project, in which I'll be monitoring the load of a truck so I can know what's going on with the load.
It's a very safety critical load, so I decided using this ARM processor. But I don't know anything about it. The first…
Other Parts Discussed in Thread: F035FLASHAPI
Hi,
Can you provide startup code for TMS470MF03107 controller and sample code of flash module?
Could you please provide the compiler manual CCS v4.6.3
Regards,
Sarada
Other Parts Discussed in Thread: TMS470MF03107 , TMS470MF04207 Dear Sir,
TMS470MF03107 go to the sleep mode. How much is the power consumption ???
I have checked this TMS470MF04207/TMS470MF03107 16/32-Bit RISC Flash Microcontroller (Rev. C) : SPNS15C…
Other Parts Discussed in Thread: TMS470MF03107 A customer is receiving this error dialog window during compile of a project (TMS470MF03107 based)
Title: "MKS Toolkit Licensing Error"
Message: " Unsupported OS Version. Contact MKS Support".
There…
Other Parts Discussed in Thread: TMS470MF06607 , TMS470MF03107 Hi
I have generated the code for TMS470066 HDK which has TMS470MF06607 microcontroller.
And i have also developed the application part for my project for the same microcontroller.
…
Mehmet,
I am confused? You asked originally for programmer information for the TMS470MF06607 but now are asking for the programmer information for the TMS470R1VF288PZA device? Are you developing with this product?
This device is NRND and currently…
Other Parts Discussed in Thread: TMS470MF03107 Hello TI
I am having issues with JTAG connection on the TMS470/570 microcontroller and CCS 5.5. I keep getting the following error.
"This path-length test uses blocks of 512 32-bit words.
The test for…
Other Parts Discussed in Thread: UNIFLASH , TMS470MF04207 , TMS470MF03107 Hello,
I am currently using UniFlash 3.1.0.00026 and I am trying to save memory from a TMS470MF04207, but it fails.
My configuration is given below:
My console log is…
Hello Benjamin, Do you need SIL3? If not, we have the TMS470M line of devices (TMS470MF06607, TMS470MF04207, TMS470MF03107) which are all pin compatible with 2 LIN instantiations. They are 80MHz Cortex M3 based devices ranging from 256KB to 640KB of flash…
Other Parts Discussed in Thread: TMS470MF03107 Hello,
I use a TMS470MF03107 to implement a LIN slave. The baudrate detection feature is set.
In the TRM, it is written :
The MBR value should be programmed to allow a maximum baud rate that is not…