Part Number: TMS570LC4357-EP Other Parts Discussed in Thread: HALCOGEN Hi, I am working on the TMS570LC4357-EP and trying to use MibSPI with DMA for transmit-only operation. I referred to the HALCoGen example (example_mibspiDma), where the transfer size…
Part Number: TMS570LC4357-EP Not able to program microcontroller as warm_reset is stuck at "0". Scan chain test is passed randomly but not able to flash the code.
What could be the conditions for setting the warm_reset to 0 by MCU?
Also please list…
Part Number: TMS570LC4357-EP What speeds do the spi interfaces run at on the TMS570LC4357-EP MCU? Does it have the capability to run at speeds slower than when it may typically run at?
Part Number: TMS570LC4357-EP Tool/software:
We are using TMS570LC4357-EP. Signal EMIF-nOE is provided on pin E12, whereas as per kit the same is available with bubble input on D12. please clarify which is correct as well as what is the significance…
Part Number: TMS570LC4357-EP Other Parts Discussed in Thread: TMS570LC4357 , HALCOGEN
Use of safety libraries for MCU TMS570LC4357 is giving all the exceptions present.
Flash self test is the only API giving the result without any exceptions
Rest…
Part Number: TMS570LC4357-EP Other Parts Discussed in Thread: HALCOGEN Hello,
I am looking to see if a spreadsheet is available to easily identify/copy the pin assignments and functions for the TI TMS5704357BGWTEP for the pinouts? thanks.
Part Number: TMS570LC4357-EP Other Parts Discussed in Thread: TMS570LC4357
Use of safety libraries for MCU TMS570LC4357 is giving all the exceptions present.
Flash self test is the only API giving the result without any exceptions
Rest of the API…
Part Number: TMS570LC4357-EP Hello, We have been working with the TMS570LC4357-EP chipset. To minimze impact of setting PLL, we applied advisory spna233b (SSWF021 #45) as linked here: Hercules PLL Advisory SSWF021#45 Workaround (Rev. B) We found that…
Part Number: TMS570LC4357-EP Dear Ti Team
First, I downloaded the FAPI_TEST_LC4357 project from the forum.
I created a new project and placed all header files and source files for FAPI_TEST_LC4357 into the new project. The compilation succeeded, but…
Part Number: TMS570LC4357-EP Hello,
I have a question on the SPIENA signal on the MibSPI interface for TMS570LC4357-EP. Is this pin only utilized if it is required by the slave device? How exactly does it differ from SPICS pins? According to the datasheet…