Part Number: TMS570LS0432 Other Parts Discussed in Thread: HALCOGEN Hi, I developed Hercules (LS0432) Fee driver code through HalCoGen, and it's linked to my CCS already. But I'm receiving error during compilation. I've resolved the familiar errors but…
Part Number: TMS570LS0432 Other Parts Discussed in Thread: TMDSEMU200-U , TMDSEMU110-U Dear Team,
can TMDSEMU110-U debugger be used? Or does it have to be TMDSEMU200-U?
Thx and regards!
Part Number: TMS570LS0432 HI,
I use TMS570 MCU CAN Bus functions.
I want do load the CAN ID and data.
how to write the code do to that?
I set the message box9 ID is 0x14EA01EF.
I set the int variable "u32temp" to read the ID,but it can work…
Part Number: TMS570LS0432 Hi,
I would like to double check the recommended decoupling caps and values for this uC.
Vccio has 4 pins and Vcc has 7 pins. Is it recommended 1 cap per pin and a bulk capacitor?
We are using minimum functionality of the…
Part Number: TMS570LS0432 Hello
I want to use mibadc ,for only one Io for adc.
I hope to trigger many times, and read the data later.means read more data.
I find mibadc is many data for more io, I want only one io for more data
How to…
Part Number: TMS570LS0432 Hello TI,
I am using TMS570LS0432, XDS200 debugger. INitially everything works. After new code chnage (code tested on TMS EVM but using XDS100v3 debugger by team member); i get following below errors but I use XDS200 instead…
Part Number: TMS570LS0432 Other Parts Discussed in Thread: HALCOGEN Hi BU experts,
My customer found 7 pcs TMS570LS0432-based board have no CAN output under low temperature (-40 °C). They did low temperature test on the failure board and I supported…
Part Number: TMS570LS0432 Hi,
Customer saw the zip in the previous thread and would like to request if the team can provide the 1738.SPI_EPROM_1224PGE.ZIP (Tried to looked into the file but once clicked it gives a message ""You do not have permission…
Part Number: TMS570LS0432 Other Parts Discussed in Thread: BQ76PL455EVM I am trying to program the TMS57004 Launchpad with the sample code provided by TI to work with the BQ76PL455EVM.
I set the RTI 100ms to update battery data, 100ms polling SCI notification…
Part Number: TMS570LS0432 The datasheet of the uC establishes a start-up and timing sequence for nPORRST vs power lines.
Is there any requirement for nRST if it is not used? Can it be pulled-up safely to the same 3.3V line as the uC power supply? Is…