Part Number: TMS570LS0914 have a board with a TMS570LS0914 processor and a USB to serial converter that can do JTAG (A CY7C65215). I would like to be able to update the FLASH via that interface.
openocd has support for the JTAG interface and for the…
Part Number: TMS570LS0914 I have a board with a TMS570LS0914 processor and a USB to serial converter that can do JTAG (A CY7C65215). I would like to be able to update the FLASH via that interface.
openocd has support for the JTAG interface and for the…
Part Number: TMS570LS0914 Other Parts Discussed in Thread: HALCOGEN Hi Team,
I am working on a TMS570LS0914 based application with the following setup:
System Configuration
MCU: TMS570LS0914
Bootloader present
Application start address: 0x00020000…
Part Number: TMS570LS0914 Other Parts Discussed in Thread: TMS570LS0714 Tool/software: Hello,
I am looking for evolution board of TMS570LS0914 . Kindly help me to get it .
Part Number: TMS570LS0914 CAN1 is not communicating after the Sleep-to-Wake-up transition, while CAN2 resumes communication successfully. Both CAN channels use the same wake-up triggers and follow the same software communication flow. Since CAN2 communication…
Part Number: TMS570LS0914 Tool/software: ESM Group3 Fault After Flash API Usage on TMS570LS0914 – APIs Run from RAM
Hi TI Community,
I'm working on the Hercules TMS570LS0914 and have encountered an ESM Group3 error after integrating and calling…
Part Number: TMS570LS0914 The TMS570LS914 N2HET1 module is used to measure the period and duty cycle of external PWM signals.
PWM input capture operates correctly on the following N2HET1 pin pairs:
N2HET1[4] and N2HET1[5] , N2HET1[12] and N2HET1[13…
Part Number: TMS570LS0914 Hello,
I am trying to write some data to flash. but the code gets crash at Fapi_setActiveFlashBank(bank0).
this happens specifiaclly bank0. before calling this function I have copied code from falsh to ram.
for writing…
Part Number: TMS570LS0914 Other Parts Discussed in Thread: HALCOGEN I'm trying to clear the error counters in the chip, but I'm not having any success. I've looked through the forums and didn't get much help.
In the error interrupt, I have the following…
Part Number: TMS570LS0914 Project description:
Trying to push firmware data from host(TMS570LS0914) to PLC chip (QCA7006) via SPI1. After excution of some commands it is going to undefEntry.
The LR is consistently pointing to this __TI_Decompress_None…