Part Number: TMS570LS1114 hi,In the Startup.c function, there is a call to the _TI_auto_init() interface function. What is the specific implementation of this function?
Thanks a lot.
Part Number: TMS570LS1114 Dear support forum,
regarding the emulated EEPROM inside the TMS570LS family, we might face issues regarding the timing requirements:
The worst case time for a sectore erase of 8 s is simply to high. Therefore, we think…
Part Number: TMS570LS1114 The program cannot run, unacceptable field reliability problems, the program can be erased, cannot be re-burned write, burn write prompt error as follows,Please help to analyze the cause
[ERROR] CortexR4: File Loader: Memory…
Part Number: TMS570LS1114 Hi:
I met some question in my code debug ,Below is My source code
#include "all_header.h"
static uint32_t Received_ID ; g_dmaCTRL g_dmaCTRLPKT; /*dma control packet configuration stack*/
#define D_COUNT 8 #define D_SIZE…
Part Number: TMS570LS1114 Hi,
is there any difference between these two apart from temperature range, AEC-Q100 and ASIL?
Are they compatible up to 160MHz and up to 105°C?
Thanks,
Tamas
Part Number: TMS570LS1114 Other Parts Discussed in Thread: SAFETI-HERCULES-DIAG-LIB-CSP Dear support forum,
we are currently confused regarding the costs of the CSPs mentioned above. From our current understanding, we might only need to buy the LDRAunit…
Part Number: TMS570LS1114 Other Parts Discussed in Thread: HALCOGEN , TMS570LC4357 Hi Experts, Good day
Currently, I have this target TMS5701114 C PGEQQ1 and need to generate Direct memory access DMA Code from Halcogen so please provide me with one…
Part Number: TMS570LS1114 I have asked the difference between 1BIT ECC of Flash and 1BIT ECC of Sram on E2E before. Due to the characteristics of Flash itself, the corrected data cannot be written to Flash, that is, the data on the original Flash address…