Part Number: TMS570LS3137 Other Parts Discussed in Thread: HALCOGEN Dear All.
I'll ask a question just in case. I have two TMS570LS3137ZWT DevKits and am testing SPI communication while using one as SPI3-Master and the other as SPI5-Slave.
Halcogen…
Part Number: TMS570LS3137 Hello,
I've been using the Profile Clock in CCS to measure performance for my TMS570LS3137.
I tried to measure the clock cycles for the below simple instructions in assembly language by keeping breakpoints.
mov r12, #0xa
strb…
Hi Furkan,
I solved very similar issue on CRC with FULL CPU Mode on below thread:
(+) TMS570LS3137: TMS570 CRC calculation - Arm-based microcontrollers forum - Arm-based microcontrollers - TI E2E support forums
-- Thanks & regards, Jagadish.
Part Number: TMS570LS3137 Hi,
We encountered an issue related executable outputs. We got executable files from a project and we checked these executable files consistent or not. Our executable .bin file size 54 kb but .hex file size is also 34 kb it no…
Part Number: TMS570LS3137 Other Parts Discussed in Thread: HALCOGEN
We are using the TMS570S3137.
We need to use NHET1[21], NHET1[23], NHET1[25] as GPIO inputs, but they don't read the value of the signal connected to them.
These signals are MUXed and…
Hi Fatih,
I use TMS570LS3137 LWIP demo. The URL for source code & CCS project is: http://git.ti.com/hercules_examples/hercules_examples/trees/master/Application/LwIP
Please refer to User Guide under docs for more details.
Part Number: TMS570LS3137 Other Parts Discussed in Thread: HALCOGEN Dear All.
I'm trying to make a watchdog using the TMS570LS3137ZWT chip. If you look at Halcogen's "Help Topics", there is an example source for implementing dwwd in "Examples".…