Part Number: TMS570LS3137-EP Other Parts Discussed in Thread: HALCOGEN Hi,
In rtiBlinky example on HalCoGen, the code gioSetPort(hetPORT1, gioGetPort(hetPORT1) ^ 0x0000001); is used to toggle HET pin 0.
What is the value to toggle other HET pins?…
Part Number: TMS570LS3137-EP Other Parts Discussed in Thread: HALCOGEN ,
I created the project in HalCoGen for the TMS570LS3137ZWT as it is the same part as the TMS570LS3137-EP functionally, with the same 337 pin NFBGA package. I have enabled the…
Part Number: TMS570LS3137-EP Hi,
Can you please tell me the sinking capability of the pin L19: DMM_DATA[0] in TMS5703137CGWTMEP?
Can it sink 330uA and what will be the approximate pin voltage when the pin is configured as output and it sinks 330uA…
Part Number: TMS570LS3137-EP I am trying to write a software installer for the TMS570. In the reference manual it mentions that the OTP flash memory starts at 0x00000000, but I am not sure where I need to start writing the program data if I am going to…
Part Number: TMS570LS3137-EP The link to download the F021 Flash API is broken. Do you know where I can download the F021 Flash API and FEE Driver?
I understand that using these libraries is the only way that we can write/read/erase data flash on the…
Part Number: TMS570LS3137-EP Hi,
I would like a communication link between two of the same microcontrollers. Could you tell me which interface type would be the fastest? It will be great if you could give me the rate of communication for different types…
Thank you, Wade. I will discuss with my team about this. In the meanwhile, can you please confirm me that TMS570LS3137-EP is available only as rev C instead of D (despite the non-EP) ? Just to exclude a missed update on the webpage. Thanks ahead. Regards…
Part Number: TMS570LS3137-EP Who do I talk to at TI for radiation test information on this part number? It is referenced in a white paper as available from manufacturer.
Part Number: TMS570LS3137-EP Hello Could you help me respond to a couple of questions from a customer
To get an idea of the data retention capability of TMS570 for our application, could you please provide a detailed graph showing the temperature/data…
Part Number: TMS570LS3137-EP We recently added some digital-inputs to the upper 16-bits of the N2HET1, and I cannot seem to read them as inputs. I actually have 6 digital-inputs on this N2HET1 -- 3 in the lower 16 bits (all work) and 3 in the upper 16…