Part Number: TMUX-24PW-EVM Other Parts Discussed in Thread: TMUX8108 Dear Technical Support Team,
I'm considering implementing and evaluating the TMUX8108PWR on the TMUX-24PW-EVM.
Is it possible to mount it using a soldering iron, and what are the…
Hi Ciaran,
I'm an engineer that primarily supports the TPS65987 products, but should be able to provide some feedback on the TMUX EVM.
What it appears you are looking for is control over the cable-orientation. The TMUXHS4446 appears to have two control…
Hi Florian,
Florian Kaffanke said: There are two SPI masters on the same bus, don't they interfere with each other? I guess not, because the SPI interface from the TPS65987D is high impedance after booting up and reading the flash only once. But this…
Hello Alon,
Can you describe your hardware and provide a schematic? You mention that the same coil works properly with LDC1614. Is this using the EVM or some other hardware? Does this also use the TMUX device?
When using single channel operation, please…
Part Number: M2-CC3351 Other Parts Discussed in Thread: CC3351 , SK-AM62-SIP , AM625 Tool/software: Hello All,
I am getting the following driver errors when streaming video for a few minutes (2-15) to the M2-CC3351 wifi module.
We plan to deploy thousands…
Part Number: TDA4VM Hi Team,
I'm porting meta-ros to yocto pro, using TDA4 project.
I added the source code as follows.
cd source
git clone -b dunfell https://github.com/ros/meta-ros.git
I added meta-ros related packages in conf/bblayer.conf
I added…