Part Number: TMUX1208-Q1 Other Parts Discussed in Thread: TMUX1208 , TMUX1108 Hi
I try to download the IBIS file of TMUX1208 to run the simulation, but it is not workable because the S1~S8 are "nc" after compare with TMUX1108.
thanks
Part Number: TMUX1208-Q1 Hello,
Does the TMUX1208QRSVRQ1 chip have powered off protection for the source inputs? I would like to know if there is a requirement to have 5V brought up on the bus before applying analog inputs to S1-S8.
Thank you
Part Number: TMUX1208-Q1 Hello Expert,
Could we leave floating at unused Sx pins? Or should we pull-up/down at unused pin from any reason(e.g. cross talk, noise coupling, ESD, etc)?
Best regards, Kazuki Kuramochi
Part Number: TMUX1308-Q1 Other Parts Discussed in Thread: TMUX1208-Q1
Dear expert,
Customer find signal flow from Sx pin to D pin. 3.3V Signal voltage dropped by around 0.1 V. Is this normal?
Is this 0.1V voltage drop fixed value? For example…
Part Number: TMUX1308-Q1 Other Parts Discussed in Thread: TMUX1208 , CD74HC4051 , TMUX1308 , , TMUX1208-Q1 e2e,
I'm considering to use MUX CD74HC4051 to expand the ADC input, what’s your recommend for this application? TMUX1208 or TMUX1308?
I checked…
Other Parts Discussed in Thread: TMUX1309 The following table helps select th e right multiplexer and switch with Low Voltage VSIGNAL =< 24V in different configurations:
Precision , Protection , Automotive , General Purpose
Configuration…
Part Number: TMUX1308 Other Parts Discussed in Thread: TMUX1108 , TMUX1208 Hi
There are 12 sets of MLX91220, which need to be connected to analog switches, such as TMUX13XX-Q1 (2pcs), but the internal resistance of conduction seems to be too large.…
Part Number: TMUX1208
Hi Team,
We understand that Typical Crosstalk are -64dB and -42dB.
We have three questions.
--------
[Q1]
Could you please let us know Max and Min values if you have any information?
[Q2]
Could you please let…
Hi Eric,
Thanks for your interest in our 8:1 muxes.
TMUX1208 is a great choice because it has a wider supply voltage range, break-before-make switching, fail-safe logic, and supports 1.8V control inputs.
I would also like to suggest taking a look…