Part Number: TMUX1308-Q1 Other Parts Discussed in Thread: TMUX1308 , , TMUX1309-Q1 When system don't power on completely, VCC of TMUX1308 is not available and high voltage level(5V) is applied on data input pin. Leakage happen under such scenario.
In…
Part Number: TMUX1308-Q1 Tool/software: I would like to select between two signals to pass from input to output (low current <50 mA ). electromechanical relay is a solution as I know normally closed (NC) and normally opened (NO) states. However, electromechanical…
Part Number: TMUX1308 Other Parts Discussed in Thread: TXU0204 , , LM324B , DRV8873 Dear All,
I want to use the TMUX1308 for 4 sensor readings via LM324B (analog) and 2 current readings (analog) from DRV8873 and 2 RPM digital signals (3V) from TXU0204…
Part Number: TMUX1308A-Q1 Other Parts Discussed in Thread: TMUX1308-Q1 , TMUX1308A , TMUX1308 Dear team,
We inform in our web site that TMUX1308A-Q1 is a drop-in replacement with upgraded performance to TMUX1308-Q1, but our customer would like our experts…
Part Number: TMUX1308-Q1 Other Parts Discussed in Thread: TMUX1308 Tool/software: I want to connect two TMUX1308 in parallel with Aurix39XX. same address pins for both and different analog pin of Aurix. Is it possible in that way thank you in advance…
Part Number: TMUX1308-Q1 Use 1V8 supplied the TMUX1308-Q1.
If ADC channel input voltage over 1.8V(like 18V, not last long ), do i need add some protection parts ? solution1: No need, connect directly solution2: add resistor in series to limit the current…
Part Number: TMUX1308-Q1 Hi team,
I would like to confirm the output(D) status of TMUX1308-Q1 when EN=High. In this case, output D will be Hi-Z and voltage could be unstable? If we need a firm Low output in this case, a pull down resistor at D is required…
Part Number: TMUX1308-Q1 Please tell me specifically what kind of abnormal behavior (i.e., behavior that is not as expected) the multiplexer exhibits when an unused source pin, which is supposed to be connected to GND, is not properly soldered and is…
Part Number: TMUX1308-Q1 Tool/software: Hello,
My customer has the following questions after reviewing the datasheet:
First question: Total time from one channel to another is t = t_break_before_make + t_transition + t_propagation_delay. Is this correct…