Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: TMUX1309 Other Parts Discussed in Thread: TMUX1209 Hi team,
Qisda have a new project for HP.
and I find some opportunity, but I am not sure if I am right or not.
Do you think TMUX1309BQBR could compete PI3USB14-ALEX.
Part Number: TMUX1309 HI team,
My customer wants to evaluate TMUX1309. And they concerns about the leakage current. If VDD=0V, and there is 5V signal on I/O pins, will that introduce any leakage current from powered I/O to VDD via internal circuit of…
Part Number: TMUX1309 Other Parts Discussed in Thread: TMUX1208 The TMUX1309 datasheets shows that Ron under the 25C and 1.8V operations condition can reach 1500ohm MAX, yet the bandwidth section shows that this part can support up to 350MHz. It's not…
Part Number: TMUX1309 Other Parts Discussed in Thread: SN74HC4852 , Hi Team,
can Pin 7 of TMUX1309 be connected to GND? Same question for SN74HC4852 if you don`t mind answering in the same thread.
Regards
Andreas
Part Number: TMUX1309-Q1 Other Parts Discussed in Thread: TLV9002-Q1 Hi team,
I don't use S1A and S1B pins and plan to connect these pin directly to GND.
Since DA and DB are both connected to the OPAMP positive terminal without any capacitor connected…
Part Number: SN65LVDS104 Other Parts Discussed in Thread: SN65LVDS22 , TMUX1309 Tool/software: I'm looking for an LVDS clock multiplexer. Essentially the opposite of the SN65LVDS104 repeater, i.e. 4:1 LVDS. Any suggestions? Thanks
Part Number: TMUX1309-Q1 Hi all,
I would like to know if TMUX1309-Q1 can be used as an I2S multiplexer. Typically, I2S uses 3 lines, such as data, clock and word select. If 2 of TMUX1309-Q1 is used, are you able to use TMUX1309-Q1 as a 1:4 multiplexer…
Part Number: TMUX1309 Hi expert,
My customer is considering TMUX1309. however their system has the condition that is supplied 3.3V to Sx at Vdd=0V.
ABS max for Sx pins is Vdd+0.5V.
Will TMUX1309 have any damage with this condition?
I found the diode…
Part Number: TMUX1309 Dear Specialists,
My customer is interested in TMUX1309.
Could you please let us know when is the RTM.
I appreiciate your great help in advance.
Best regards,
Shinichi