Part Number: TMUX136 Other Parts Discussed in Thread: TS3USB3000 Hi team
Do we have mux suitable for the following two type of signals?
Input#1: 6.5Gbps differential signal (from FPGA Serdes)
Input#2 : <100Hz 3.3V LVCMOS signal (Video VS signal)
…
Part Number: TMUX136 1. What is the difference in bandwidth between a single tmux136 chip and three tmux136 chips in series, or the bandwidth is not affected by the multi-cascade of chips.
2. The bandwidth (-3dB) written in the specification: 6.1GHz.…
Part Number: TMUX136 Other Parts Discussed in Thread: DP83867CS , I intend to use TMUX136 in my design with DP83867CS (on the SGMII interface). Request you to suggest whether capacitive coupling is needed on both the sides of mux or single side is sufficient…
Part Number: TMUX136 Other Parts Discussed in Thread: SN74AXC4T245 Hi TI team,
I would like to ask about unexpected output of using TMUX136.
I have the clock generator at the input of COM1 , with the EN_N is controlled by the dip switch to turn on/off…
Part Number: TMUX136 Dear team,
Customer want to use TMUX136 in 1.8V I2C application.
Can we use 3.3V power level on VCC and connect 1.8V I2C signal at mux in/out pins?
Thanks.
Regards,
Ben
Part Number: TMUX136 Other Parts Discussed in Thread: TMUX1072 Hi,
It is noticed that VIH is 1.3V (min) for SEL and EN_bar.
What is the input voltage range for COM1/2 ?
Part Number: TMUX136 Dear Engineers,
System is having two SPI bus where three devices on single SPI (with individual CS) for 50Mhz & 75Mhz are attached.
Where SPI MISO is shared with multiple slave devices and based on CS, SDO will be tristate. system…
Part Number: TMUX136 Hi All,
I am looking for a coupon board for device TMUX136RSER [UQFN/RSE pkg] to solder this part or worst case an EVM board. Thanks!!
Part Number: TMUX136 Hello Team,
My customer is looking forward to use our TMUX13, however they wanted to know any noise that associated with it and its specification.
Looking forward to your response.
Regards,
Renan
Part Number: TMUX136
Hello team,
I proposed this part as the switch of I3C signal, so would you like to help us check whether it has any issue using this part?
Thanks.
Antony