Part Number: TMUX4052 Other Parts Discussed in Thread: CD4052B , CD74HCT4052 Hi E2E,
Is there similar or P2P device with NXP/74HC052DB ?
Or is there component with smaller footprint and can design an adapter (if the speed of replacement device is…
Part Number: TMUX4052 Other Parts Discussed in Thread: TMUX1308 Dear Experts:
We will use TMUX4052 as the channel switcher for analog ADC sampling. So its Ron resistance is circuital. The datasheet shows then typ value is 60 ohm at 25C, 24vdc, 1mA current…
Part Number: TMUX4052 Tool/software: Dear sir:
For use TMUX4052, the VDD use 12V input.
When select pin (A0 ans A1) control by GPIO (3.3V MCU), the 3.3V will be high (ture table 1) or need use 12V for high?
Thanks for the help.
by Steve.Yeh
Part Number: TMUX4052 Other Parts Discussed in Thread: SN74LV4052A Hi,
Customer raised a question about TMUX4052. We know that you have modified supply range from 3V~12V to 5V~24V. Could you help to check what is the supply voltage with the data code…
Part Number: TMUX4052 Tool/software: Hi Expert,
My customer is using TMUX4052 to measure 4ch current signals. But they find that when four input channels all have signals and the selected output channel will have a crosstalk. And when there is only…
Part Number: TMUX4052 Other Parts Discussed in Thread: TPS65132 , , TMUX6236 , TMUX7436F Tool/software: Hi team,
Can MUX4052 support differential signals?
use TPS65132 provide +-6V and signal speed is 5MHz and +-5V
block as below. pls help to check…
Part Number: TMUX4052 In our design we are using the multiplexer part TMUX4052PWR. We are going to use VDD Pin (Positive power supply) for single power supply operation. Another Power Supply VSS pin is dedicated for the negative power supply. What should…
Part Number: TMUX4052 Tool/software: Hello all,
I would like to ask for clarification on the following note taken from the TMUX405x datasheet[1]. It is mentioned on page 7 (Absolute Maximum Ratings).
(3) To avoid drawing excess current from VDD, or…
Part Number: TMUX4052-Q1 Other Parts Discussed in Thread: TMUX4052 Hi team,
Do you have the simulation model of TMUX4052-Q1, could you send it to me?
Thanks!