Part Number: TMUX6209 Other Parts Discussed in Thread: TMUX1209 Hi,
I want to connect MCU single CAN port to interface multiple CAN modules. Is this possible by using TMUX1209/6209/7209 to interface between single CAN to multiple CANs. Is there any…
Part Number: TMUX6209 Tool/software: Hi, I’m planning to use the TMUX6209 to measure the cell voltages of a multi-series lithium-ion battery pack. The mux itself will be powered from the same battery stack.
Can each analog input (Sx/Dx pin) reach…
Part Number: TMUX6209 Other Parts Discussed in Thread: TMUX6208 Hello!
Datasheet for TMUX6209 (Available both from https://www.ti.com/lit/ds/symlink/tmux6208.pdf and https://www.ti.com/lit/ds/symlink/tmux6209.pdf ) states that logic pins have 4M pull…
Part Number: TMUX6209 Other Parts Discussed in Thread: TMUX4827 Hi,
I want to measure the current flowing through the 9V power rail. I have connected a Sense resistor in series of the rail and both end of the resistor is connected to S1A & S1B terminal…
Part Number: TMUX6209 Hello Team,
Can you confirm if the device TMUX6209 (TMUX620x family) is latch-up immune?
The datasheet section 9.3.6 on page 32 says the part is latch-up immune, however, (1) the description and datasheet name for TMUX620x does…
Part Number: TMUX4819 Other Parts Discussed in Thread: TMUX6209 , TMUX6111 , Hi TI experts,
Below is the snapshot of our current design, we wab to replace MAX14778ETP+. We survey TMUX6209, TMUX6111,TS3A50, however, these parts need dual power input…
Part Number: SN74CBT16214C Other Parts Discussed in Thread: TMUX6209 , TMUX6234 , TMUX4051 Hello E2E Experts,
Currently we working on one configuration where we need the similar product like SN74CBT16214CDGGR where the selection of input channels are…
Hi Gabriele,
Gabriele Vegetali said: one thing i want to ask you is: if the signals instead are not so synchronized (so maybe some input ramp faster than the power supply Vcc pin, even with very small voltage difference), is there a possibility that…
Hi Jade,
The best 8:1 muxes that can operate at 125C and take 5V power would either be TMUX1108 , which has a 66mA max continuous current or TMUX6208 , which has a 99mA continuous current max for the RUM package when powered with 5V at 125C.
The best…
Part Number: TMUX1072 Other Parts Discussed in Thread: TMUX6209
Hello,
I am currently in search of a high voltage tolerance mux or switch for our wireless power transmission system. This component will be connected to a single coil and will alternate…