Hi Satya,
You do not need to do any modification on the DSS driver side. You will need to take care of software need for ADV3003 (if any).
If you are following the dts settings from TI EVM, then you need to modify the dts settings to remove tpd12s015…
Part Number: AM67A Other Parts Discussed in Thread: SN65DSI86 , , AM62P , TPD12S015 , DLPC3433 , SN65DSI83 , TFP410
eDP Bridge SN65DSI86: SoC: AM67A Embedded DisplayPort Bridge: SN65DSI86
I am working on a custom embedded board based on the AM67A…
Which Linux SDK is this?
In latest TI SDK the HDMI is already enabled, see am57xx0beagle-x15-common.dtsi:
aliases {
rtc0 = &mcp_rtc;
rtc1 = &tps659038_rtc;
rtc2 = &rtc;
display0 = &hdmi0;
sound0 = &sound0;
sound1 = &hdmi;
};
…
Part Number: AM5728 Other Parts Discussed in Thread: TPD12S015 , DS90CR217
Tool/software: Linux
Hello All,
Environment setup using:
OS: ubuntu 16.04
Ti-SDK:ti-processor-sdk-linux-am57xx-evm-04.02.00.09
I'm integrating 10.4"(800x600) display…
Tom,
Thank you
1. We are connecting the HDMI display through connector and a long cable . This is the reason to include ADV3003 buffer in between AM5728 HDMI out and connector.
2. We have a fixed installation for HDMI display. we learnt that by configuring…
Hi manisha ; Thanks for your help; Can you please check the below dtsi changes are ok for HDMI? or still we missing something? aliases { rtc0 = &tps659038_rtc; rtc1 = &rtc; display0 = &hdmi0; }; hdmi0: connector@0 { compatible = "hdmi-connector"; label…
Part Number: DRA71XEVM Other Parts Discussed in Thread: TPD12S015 Tool/software: Linux Hi,
I am using SDK vision ti-processor-sdk-linux-automotive-dra7xx-evm-03_02_00_03 and JACINTO 6 ENTRY/RSP EVM REV C. And below is my usecase,
I am using dra71…
Hello zheng,
Please, check the am57xx-evm-reva3.dts which includes am57xx-beagle-x15-revb1.dts and am57xx-beagle-x15-revb1.dts contains &tpd12s015 node where the <&gpio7 12 GPIO_ACTIVE_HIGH>; /* gpio7_12/sp1_cs2, HPD */ is initialised.
Best regards…
Part Number: AM5728 Other Parts Discussed in Thread: TPD12S015
Tool/software: Linux
I'm working with yocto (rocko) linux-ti-staging 4.9.69 on a beagle x15 rev C board.
I have been attempting to disable the device tree nodes of x15 features I do…