Part Number: ESD451 Other Parts Discussed in Thread: TPD1E0B04 , TPD1E01B04 Tool/software: Hi,
Does ESD451 suitable for Thunder bolt 4 or 5 application?
I saw the IO capacitance is 0.5pF. Or TPD1E0B04 is better suggestion?
Does we have any ESD device…
Part Number: TPD1E01B04 Other Parts Discussed in Thread: TPD1E0B04 Tool/software: Hi,
can TPD1E01B04 support thunderbolt 5 application? if not, any device can support?
Part Number: TSER9615 Other Parts Discussed in Thread: TDES9640 , , TSER953 , TPD1E0B04 , TPD1E01B04 Tool/software: Dear Support,
we have a few question regarding using TSER9615 ( 7.5G) and TSER953 ( 4G) connected to TDES9640 via STP ( no power over…
Part Number: TPD4E02B04 Other Parts Discussed in Thread: TPD1E0B04 , TPD1E01B04 Tool/software: I check the Differential Insertion Loss on the datasheet that is 3dB@ 10GHz.
Does TPD4E02B04 can be used on USB3 gen2 (10Gbps)??
And TI support other ESD…
Part Number: ESDS314 Other Parts Discussed in Thread: TPD1E0B04 , TPD1E01B04 Tool/software: Hi team,
The ESDS314 supports high-speed interfaces up to 5Gbps, but are there any ESD protection products that support 25Gbps high-speed Ethernet?
If not…
Back to Interface Home Page
UART Protection
Highlights:
Lower speed serial data transfer interface
Operating lines: GND, ±TX, ±RX
Datalines (±Tx, ±Rx) Operating voltage: 3.3V, recommended Vbr > 3.6V
Data rates up to 5Mbps
TI…
Other Parts Discussed in Thread: TPD1E0B04 hello Expert,
Do you have any experience for the surge protection of RF antenna and RF board?
I know we can add a surge protector likes as below with outdoor antenna, but how about RF board?
RF trace should…
Part Number: TPD1E0B04EVM Other Parts Discussed in Thread: TPD1E0B04 Hi E2E, Do we have the Gerber files for the TPD1E0B04 Evaluation Module? Regards, Carlo
Part Number: CC1312R Other Parts Discussed in Thread: TPD1E0B04 Hello, What is the ESD clamping voltage of on the onchip protection for the CC1312 IC? We are in the process of adding board level esd protection and want to make sure that our board level…