Part Number: TPD1E1B04 Other Parts Discussed in Thread: TPD1E04U04 Hi,
Can any body suggest changes to be done while doing ESD test as our LCD is failing even with TPD1E1B04 diodes mounted on mipi lines of the LCD & also Type C input connector (data…
Part Number: TPD1E1B04 Other Parts Discussed in Thread: ESD351 Hello
My customer is considering ESD Protection devices for SPI communication lines.
They are testing it in one way using TI's TVS Diode TPD1E1B04.
Is there any new technology product…
Part Number: TPD1E1B04 Other Parts Discussed in Thread: TPD1E0B04 Hi TI Team,
We are Taiwanese team that supports TI products.
At present, we talk about the ESD solution with our customers in Taiwan.,
Since this application is an antenna related…
Part Number: TPD1E1B04 Other Parts Discussed in Thread: AM3359 , , TPD1E04U04 Hi
I have a query regarding TVS diode selection for AM3359 Processor reset switch.
I am planning to use TPD1E1B04 ESD diode.
However, clamping voltage for this device…
Kevin,
I apologize for the delay in response.
So I misunderstood from your first question I thought you meant that the TPD1E1B04 did not protect. I believe that it will protect and I believe that the reason why the 0603ESDA-MLP did not protect was because…
Back to Interface Home Page
UART Protection
Highlights:
Lower speed serial data transfer interface
Operating lines: GND, ±TX, ±RX
Datalines (±Tx, ±Rx) Operating voltage: 3.3V, recommended Vbr > 3.6V
Data rates up to 5Mbps
TI…
Other Parts Discussed in Thread: TPD1E1B04 , ESDS302 Hi Team
I am looking for ESD protection at 3.3 and 5V, I have a doubt regarding the selection of part is that if the reverse standoff voltage is 5V then in general clamping voltage will be more than…
Hello Inho,
TPD1E1B04 would be a much better fit for this application. You want you your Vrwm to be as close to the normal operating voltage of the line as possible without it going under. In this case, the max voltage the line should see is 3.6 V…
Hi Alex,
For both of those devices, they have 15kV HBM for the bus pins, which for LVDS receivers is just the A and B pins. I am seeing that table you shared in both device datasheets, and they both describe the devices having 15kV HBM for only the…